×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 52310936, Entry date: 12/01/2014
(2)
Rate

SIMATIC IPC with Intel® AMT: Diagnostics and Remote Maintenance of SIMATIC Industrial PCs

  • Entry
  • Associated product(s)
The increasing worldwide distribution of plants increases the demand for accessing automation components, e.g. SIMATIC industrial PCs (IPCs) in remote plants.

To be able to use the remote access effectively, it should also be possible for a SIMATIC IPC that is switched-off or no longer operating. A remote operator shall be able to use the same functions as an operator directly in front of the SIMATIC IPC. In the service case, this may avoid operation on site and save time and costs.


Figure 01

Solution
SIMATIC IPC enables realizing remote access via the Intel® AMT technology. Independent of the state of the system, the user performing remote maintenance is thus provided with all the functions that an operator sitting directly in front of the IPC would also have.





Downloads
The documentation contains all necessary configuration steps to configure a SIMATIC IPC for the use of Intel® Active Management Technology
  Documentation (1,7 MB)

Last Changes
Update (current hardware)

Additional Keywords
E-learning, tutorial, teaser, example, demo, Webcast, multimedia demonstration system, MMVS, film, screencast, VNC, RDP, Remote Desktop, KVM, Management Engine, BIOS extension, Remote Manager, Manageability Director, 82577LM, Intel® Active Management Technology Developer Tool Kit (AMT DTK), remote access, remote maintenance, service, worldwide, global, remote, SIMATIC Remote Management, teleservice, tele service, remote access, telecontrol


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.