×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 52329908, Entry date: 09/07/2017
(0)
Rate

Acknowledgement of WinCC V7 Messages with Forced Comments

  • Entry
  • Associated product(s)
Expands the message function of WinCC by an additional acknowledgement function with comment.
In the pharmaceutical branch and the food and beverage sector the documentation of operator actions is becoming increasingly important. The documentation of production processes is to ensures that all operator actions are comprehensible.
In this context it is to be understood what user has acknowledged a message when and why. This information is to be displayed and archived in the control system.

Solution  
The application example expands the message function of WinCC by an additional acknowledgement function with comment. These additional comments are mandatory, they have to be used. It is not possible to acknowledge the messages with out a comment.

Not all messages have to be acknowledged with comment. They are defined through a certain message class.
If a message is acknowledged with mandatory comment, an additional dialog (WinCC picture window) appears first. In this dialog box, the comment is assigned.

Through an additionally generated operator message, the comment is stored in the message archive. The correlation between message and operator message can be made through date, time and message text. User and comment are also stored in the operator message.




 

Downloads
 Documentation (1,9 MB)
 Registrierung notwendig  Example project (18,9 MB)

Last modification
Update to WinCC V7.4

Additional Keywords
AlarmControl, comment, messages, forced comment, ForecdComment


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.