Entry type: FAQ, Entry ID: 54163658, Entry date: 07/01/2013
(12)
Rate

How do you update the hardware catalog in STEP 7 (TIA Portal)?

  • Entry
  • Associated product(s)

Instructions
STEP 7 (TIA Portal) provides the option of updating your hardware catalog. The following entries include downloads for extending the hardware catalog of your version of STEP 7 (TIA Portal). The downloads contain the software components (Support Packages) needed for the modules and can be transferred to a PC with STEP 7 Professional or STEP 7 Basic using a memory stick, for example.

  • Please go to Entry ID 72341852 for downloading the Support Packages for STEP 7 (TIA Portal) V12.
  • Please go to Entry ID 54164095 for downloading the Support Packages for STEP 7 (TIA Portal) V11.

The following table describes you how you can use the download of the Support Packages (HSPs) to update your hardware catalog.
 

No. Procedure
1

Preparation
In the TIA Portal you open the page with the Support Packages for the Hardware Catalog and then click the required download icon. Unpack the *.zip file and copy the enclosed *.isp12 files into a directory to which you have access with STEP 7 Basic or Professional.

Note
Pay attention to the software requirements specified for each Support Package (for example "for STEP 7 Professional V12" means that at least STEP 7 Professional V12 or a higher Service Pack of the same version must be installed).

  • Hardware Support Packages with the file extension "*.isp12" are for STEP 7 (TIA Portal) V12.
  • Hardware Support Packages with the file extension "*.isp11" are for STEP 7 (TIA Portal) V11.
2 Open the TIA Portal and switch to Project View.
3 Use the "Options > Support Packages" menu command to open the "Detailed information" dialog. When this dialog opens, the "Support Package Installation" tab is selected by default and the Support Packages already installed are shown in the right window.
4 Click the "Add from file system" button and navigate to the directory in which you have stored the downloaded *.isp12 files.
5 Select the required *.isp12 file.


Fig. 01

In this example we have selected the *.isp12 file of the HSP_V12_0050.

6 The HSP file for the installation is now displayed in the "Detailed information" dialog. The "Installed" column still indicates "No" for this HSP. Select the HSP file as shown in Fig. 02 and click on the "Install" button.


Fig. 02

7 Click "Continue" in the dialog that follows to start the installation.


Fig. 03

Note on STEP 7 (TIA Portal) V11
In STEP 7 (TIA Portal) V11 a message requesting you to close all instances appears instead of the dialog shown in Fig. 03. In this case you close all the open windows of the TIA Portal except the Installation window. The "Continue" button is then enabled. Click "Continue" to start the installation.

8 At the end of the installation a message is displayed indicating that the installation has been completed successfully. Click the "Finish" button and restart the TIA Portal. Now your hardware catalog in the TIA Portal is up to date. If you reopen the "Detailed information" dialog in the TIA Portal, the "Installed" column now indicates "Yes" for the HSP file.

Creation environment
The pictures in this FAQ response were created with STEP 7 V12.

Additional Keywords
HSP file, Module catalog, Hardware configuration, Hardware update, Hardware configuration, Upgrade

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster