×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 54473263, Entry date: 11/02/2011
(0)
Rate

Delivery release Telecontrol Server Basic V2.0 + Hotfix 1 (V2.0.0.1)

  • Entry
  • Associated product(s)

 

The Telecontrol Server Basic V2.0 incl. Hotfix 1 software is now available for delivery ex warehouse.

 

 

1. Product description

The new Telecontrol Server Basic software which has been available since July 15, 2011 ( ProdIS entry 51065116) connects up to 5,000 SIMATIC S7 controllers via GSM/GPRS telecommunications standard with a control center. It can be used for affordable implementation of telecontrol solutions in the areas logistics, maintenance and energy optimization.

 

Version V2.0 incl. Hotfix 1 (V2.0.0.1) is now available for delivery ex warehouse.

This Hotfix corrects the following behavior:

There may have been some rare, provider-specific instances of telegram errors with segmented data telegrams (>1,024 byte) that went undetected. Telegrams were not discarded but forwarded for processing. These transmission errors are securely detected with Hotfix 1.

 

2. Ordering data

Product name

Order number

TELECONTROL SERVER BASIC 8

6NH9910-0AA20-0AA0

TELECONTROL SERVER BASIC 64

6NH9910-0AA20-0AB0

TELECONTROL SERVER BASIC 256

6NH9910-0AA20-0AC0

TELECONTROL SERVER BASIC 1.000

6NH9910-0AA20-0AD0

TELECONTROL SERVER BASIC 5.000

6NH9910-0AA20-0AE0

 

3. Other

If you own a valid license of the Telecontrol Server Basic V2.0 software, use the Customer Support (I IA AS CS1, contact form) to order Hotfix 1.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.