×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 54992004, Entry date: 06/26/2019
(60)
Rate

SIZER for Siemens Drives

  • Entry
  • Associated product(s)
This contains the current SIZER versions.

Disclaimer of liability

Siemens does not assume any liability - irrespective of the legal grounds - especially for faults in the tool unless the same is to be attributed to us, for example, for willful damage, gross negligence, damage to life, body or health, taking over of a procurement guarantee, willful concealment of defects or violation of important contractual liability. This does not entail a change in the burden of proof to your disadvantage.

Important information

As of version V3.6, the CAD Creator is no longer part of the scope of delivery of SIZER for Siemens Drives. To use the CAD functionality, CAD Creator (as of V1.7.1) must be installed on the PC.
You can download CAD CREATOR and obtain information about it at 57218443.

Security information

Siemens offers products and solutions with Industrial Security functions, which support the secure operation of plants, systems, machines and networks.

In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art Industrial Security concept. Siemens’ products and solutions only form one element of such a concept.

Customer is responsible to prevent unauthorized access to its plants, systems, machines and networks. Systems, machines and components should only be connected to the enterprise network or the internet if and to the extent necessary and with appropriate security measures (e.g. use of firewalls and network segmentation) in place.

In addition, Siemens recommendations on appropriate safeguards should be observed. Further information on Industrial Security can be found at http://www.siemens.com/industrialsecurity.

Siemens products and solutions undergo continuous development to make them even more secure. Siemens strongly recommends to apply product updates as soon as available and to always use the latest product versions. The use of outdated versions or versions that are no longer supported can increase the risk of cyber threats.

To stay informed about product updates, subscribe to the Siemens Industrial Security RSS Feed at http://www.siemens.com/industrialsecurity.

Notice

Check the size of the zip files after downloading (1 MB corresponds to 1024 KB). The correct file sizes are specified.

Minimum system requirements

  • PG or PC, Pentium™ III min. 800 MHz (recommended > 1 GHz) 512 MB RAM (recommended > 1 GB)
  • At least 2 GB free hard disk space.
  • Additional 100 MB free hard disk space on the Windows system drive
  • Monitor resolution, 1024x768 pixels
  • Windows 7 (32/64-bit) Professional, Enterprise, Ultimate, Home
  • Windows 8.1 (32/64 bit) Professional, Enterprise, Ultimate, Home
  • Microsoft Office 2003/2007/2010/2013/2016

  • Windows 365

  • Microsoft Internet Explorer V8.0
  • Microsoft .NET Framework 2.0
  • OpenGL 2.1
  • Windows 10 Enterprise 64 Bit
  • Windows 10 Professional 64 Bit


SIZER for Siemens Drives V3.20

SIZER for Siemens Drives V3.20 (current version)
SIZER for Siemens Drives V3.20 Registrierung notwendig  SIZER_V3_20.zip (698,1 MB) 
 Registrierung notwendig  SIZER_V3_20_CAD.zip (135,7 MB) 
  What_is_new_V_3_20.pdf (134,8 KB) 
  Registrierung notwendig  Sizer_3.20__READMEOSS (1,9 MB) 

The following installation versions are available

  • Installing SIZER without dimension drawing generators
    To do this, download the "SIZER_V3_20.zip" file, unzip it and then start the setup.exe program.
    Important note
    The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup.
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
    Download the "SIZER_V3_20.zip" and  "SIZER_V3_20_CAD.zip" and unpack them to a common directory.
    Start the setup.exe program in the uppermost directory.
    Note
    A subsequent installation of the dimension drawing generators is also supported using this process.

Data update package V5.1 for SIZER V3.19

Data update package V5.1 for SIZER V3.19
Data update package

 Registrierung notwendig  SIZER_V3_19_DB_V5_1.zip (9,2 MB)

  What_is_new_V_3_19_Datenupdate_5_1.pdf (103,9 KB)

Requirements

SIZER V3.19 is installed.

Installation

  1. Unzip the ZIP file
  2. Double-click the unzipped data update package "SIZER_V3_19_DB_V5_1.szupg"

SIZER for Siemens Drives V3.19

SIZER for Siemens Drives V3.19 (current version)
SIZER for Siemens Drives V3.19 Registrierung notwendig  SIZER_V3_19.zip (699,7 MB)
 Registrierung notwendig  SIZER_V3_19_CAD.zip (135,7 MB) 
 Registrierung notwendig  What_is_new_V_3_19.pdf (112,2 KB) 
  Registrierung notwendig  SizerforSiemensDrives__READMEOSS_2018-11-30__14-11-02.html (1,9 MB) 

The following installation versions are available

  • Installing SIZER without dimension drawing generators
    To do this, download the "SIZER_V3_19.zip" file, unzip it and then start the setup.exe program.
    Important note
    The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup.
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
    Download the "SIZER_V3_19.zip" and  "SIZER_V3_19_CAD.zip" and unpack them to a common directory.
    Start the setup.exe program in the uppermost directory.
    Note
    A subsequent installation of the dimension drawing generators is also supported using this process.

Data update package V4.1 for SIZER V3.18

Data update package V4.1 for SIZER V3.18
Data update package

  Registrierung notwendig  SIZER_V3_18_DB_V4_1.zip (9,1 MB) 

 Registrierung notwendig  Data_Update_V3.18_DB_V4.1_ReleaseNotes.pdf (10,9 KB)

Requirements

SIZER V3.18 is installed.

Installation

  1. Unzip the ZIP file
  2. Double-click the unzipped data update package "SIZER_V3_18_DB_V4_1.szupg"


SIZER for Siemens Drives V3.18

SIZER for Siemens Drives V3.18 
SIZER for Siemens Drives V3.18 Registrierung notwendig  SIZER_V3_18.zip (701,3 MB) 
 Registrierung notwendig  SIZER_V3_18_CAD.zip (135,7 MB) 
 Registrierung notwendig  What_is_new_in_V3.18.pdf (84,1 KB) 
  Registrierung notwendig  Readme_OSS.zip (3,0 MB) 

The following installation versions are available

  • Installing SIZER without dimension drawing generators
    To do this, download the "SIZER_V3_18.zip" file, unzip it and then start the setup.exe program.
    Important note
    The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup.
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
    Download the "SIZER_V3_18.zip" and  "SIZER_V3_18_CAD.zip" and unpack them to a common directory.
    Start the setup.exe program in the uppermost directory.
    Note
    A subsequent installation of the dimension drawing generators is also supported using this process.


Data update package V3.1 for SIZER V3.17

Data update package V3.1 for SIZER V3.17
Data update package  Registrierung notwendig SIZER_V3_17_DB_V3_1.zip (8.9 MB)

Requirements

SIZER V3.17 is installed.

Installation

  1. Unzip the ZIP file
  2. Double-click the unzipped data update package "SIZER_V3_17_DB_V3_1.szupg"

Content

New products that have been included

  • 1FT7117, AH 100, High Dynamic
  • Note: SIMOTICS S-1FT7117-7..71-.L.0 - Z L06 servomotors are available in the following combinations:
    • with rated speeds of 2000 and 3000 rpm
    • with AM24DQI encoder (24 bit absolute encoder, multiturn with M17 signal connection)
    • DRIVE-CLiQ signal cables in conjunction with M17 signal connection are not supported in SIZER.
    • with brake, in shaft and flange accuracy tolerance N
    • with degree of protection IP64 (IP54 with fan) with vibration quantity level A
    • with option L06 (for increased shock load)
    • the outlet direction for the fan connector must be predefined for the forced-ventilation version (option Q4.)
  • For SIMOTICS GP/SD-1LG6 motors, versions "MA" and "MB" (9th and 10th position of the Article No.), the following encoders are approved and can be mounted:
    • H57 - rotary pulse encoder 1XP8001-1 (HTL)
    • H58 - rotary pulse encoder 1XP8001-2 (TTL)
    • H70 - rotary pulse encoder LL 861 900 220
    • H72 - rotary pulse encoder HOG 9 D 1024 I
    • H73 - rotary pulse encoder HOG 10 D 1024 I
  • SINAMICS G120, PM240-2, push through
  • The following article numbers are included again:
    • SIMOTICS GP-1LE1 (0; 5; 6) 03-1CC0.-....
    • SIMOTICS GP-1LE1 (0; 5; 6) 23-1CC0.-....
    • SIMOTICS GP-1LE1 (0; 5; 6) 43-1AA6.-....
Data updates
  • SIMOTICS S-1FK7 correction of the article number LP + gearbox: SIMOTICS S-1FK7022-5AK74-1HG3-Z V42
  • SIMOTICS S-1FT7, SH132, non-ventilated, characteristics have been corrected
  • SIMOTICS L-1FN3
    • The following linear motors have been added:
      • SIMOTICS L-1FN3600-4NA70
      • SIMOTICS L-1FN3600-2WB00
    • Characteristics and loss data have been revised
    • Changing over to Pt1000
  • MOTION CONNECT: Incorrect extension cable corrected
  • SINAMICS G120, PM250, standard power loss added
  • SINAMICS G120 cable lengths, circuit breakers and fuses updated
  • 60 Hz data of IEC/NEMA (Eagle Line) motors has been corrected. The previously saved IEC 60 Hz data have been replaced by the NEMA 60 Hz data relevant for these motors.
  • For converter operation, SIMOTICS GP/SD-1LE1 motors are only approved/certified for voltages of up to 480 V. As a consequence, motors with voltages of 575 V up to 690 V are locked and cannot be selected.
  • At the present time, standard SIMOTICS GP/SD-1LE1 motors in the 500 V voltage level are permitted for converter operation; this means that SIMOGEAR 2KJ geared motors are still available for 500 V. However, the 500 V voltage level is not permitted for standard SIMOTICS GP/SD-1LE1 motors for converter operation.


SIZER V3.17 Hotfix 1 (HF1)

SIZER V3.17 Hotfix 1 (HF1) 
Hotfix 1  Registrierung notwendig  SIZER_V3_17_HF1.zip (10.1 MB) 

Requirements

SIZER V3.17 is installed.

Installation

  1. Unzip the ZIP file
  2. Double-click on the "Update.exe" file

Content

Hotfix 1 for SIZER V3.17 resolves the following problems:

  • NX10 and NX15 options - that can be selected for SINUMERIK 828D - have been corrected, if the "Advanced" and "Basic" software options
  • Configuring SIMOGEAR 2KJ motors in the DT Configurator resulted in an error if the motor was originally created in a SIZER project in a SIZER version before 3.17 - and then further processed using SIZER V3.17.


SIZER for Siemens Drives V3.17

SIZER for Siemens Drives V3.17
SIZER for Siemens Drives V3.17 Registrierung notwendig SIZER_V3_17.zip (698.3 MB)
 Registrierung notwendig SIZER_V3_17_CAD.zip (135.7 MB) 
 LicenseSummary.htm_comb.zip (4.0 MB) 

 What is new in SIZER V3.17?

  • Motors, encoders and gearboxes
    • Inclusion of geared motors for suspended monorails (overhead conveyors)
    • SIMOGEAR portfolio extended to include single-stage worm geared motors
    • SIMOTICS XP 1MB1 included
    • Changes to the SIMOTICS GP/SD 1LE1 portfolio
      • SIMOTICS GP/SD 1LE1 motors can no longer be selected and dimensioned for operation with SINAMICS G110M
      • The M_stall/M_rated factor has been corrected for some 60 Hz versions
      • Default setting of the shipping connection (M01, M02) has been removed
      • Terminal box position "at the bottom" has been added (16th position of the article number = 7) for permitted shaft height
      • Update of the assignment of versions to aluminum and cast iron series
      • Update of the assignment for the enable signal on the line supply system / motor starter
    • Portfolio adjustments for SIMOTICS FD type of construction with/without protective cover
    • Portfolio adjustments for SIMOTICS GP/SD VSD10 line with addition of 2-pole versions
    • Extension of the display values in the SIMOGEAR motor dialog with the addition of rated gearbox torque and cantilever forces
    • Support for worldwide winding for SIMOGEAR
    • Configuration option for additional SIMOTICS S-1FG1 settings such as manual brake release and terminal boxes.
    • Portfolio corrections for SIMOTICS T-1FW6 natural cooling
    • Portfolio adjustments for SIMOTICS S-1PH8 for Pt1000
    • Data update for SIMOTICS M-1FE1
    • Various small data updates partially already included in the data update package for V3.16.
  • Drives / motor starters
    • Allow group drives for SINAMICS G120 and G120D
    • Circuit breakers for SINAMICS G120D have been updated
    • For SINAMICS S120 chassis SLM, the pre-charging limits have been adapted according to the Configuration Manual. In addition, the current values have been updated for the two SINAMICS Motor Modules 6SL3325-1TG41-6AP3 and 6SL3725-1TG41-6AP3.
    • Adjustment of the pulse frequency and temperature derating characteristic for the 7.5 kW Power Module for the SINAMICS G120D.
    • Input option for a pulse frequency derating for the SINAMICS G120 and G120D portfolio.
    • Update of the SINAMICS C/D type Motor Module with 24 A, 45 A and 60 A.
    • Update of the SINAMICS G120 portfolio with the addition of IOP-2 and IOP-2 handheld as well as fuses.
    • Update of the SINAMICS ET 200SP portfolio with the addition of motor starters up to 12 A.
    • Various small data updates partially already included in the data update package for V3.16.
  • Controls
    • Support of the CNC SW4.8 for SINUMERIK 840Dsl / 828D including new software options
    • Support for additional SINUMERIK operator components such as TOP panel, MCP 398C, SIMATIC IFP, IPC 427E
    • SINUMERIK 828D: Analog output configurable on PPU
    • SIMATIC S7-1500: Adjustment of the selection criteria (standard/T-CPU)
  • Additional functions
    • Input option for third-party products extended
    • For the SIMOGEAR portfolio, the new DT Configurator is called for further configuration


SIZER for Siemens Drives V3.16

Here you can find version V3.16 of the SIZER engineering tool for drive systems (SINAMICS, MICROMASTER, DYNAVERT T and SIMATIC ET 200 FC), motor starters and control systems (SINUMERIK, SIMOTION and SIMATIC Technology).

Third-party software licensing conditions and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the Readme_OSS.pdf file.

Special note for resellers

The information and the license conditions in the Readme_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  Readme_V3-16_OSS.htm (2.4 MB)


 SIZER for Siemens Drives V3.16
 SIZER for Siemens Drives V3.16

  Registrierung notwendig  SIZER_V3_16.zip (693.7 MB)

  Registrierung notwendig  SIZER_V3_16_CAD.zip (135.7 MB) 

SIZER can be used free of charge. A nominal order processing fee is charged for the DVD. The software can be used without entering a license key. However, for legal licensing reasons, you should be in possession of a SIZER license certificate (any version). If you do not have a license, you can also order the current SIZER version including the license certificate on a DVD. Article number: 6SL3070-0AA00-0AG0

The readme file contains important information on how to use the tool.

The following installation versions are available

  • Installing SIZER without dimension drawing generators
    • To do this, download the "SIZER_V3_16.zip" file, unzip it and then start the setup.exe program.
      Important note: The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup.
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
  • Download the "SIZER_V3_16.zip" and  "SIZER_V3_16_CAD.zip" and unpack them to a common directory.
  • Start the setup.exe program in the uppermost directory.
    Note
    A subsequent installation of the dimension drawing generators is also supported using this process.


Data update package V2.1 for SIZER V3.16

Data update package V2.1 for SIZER V3.16
 Data update package  Registrierung notwendig  SIZER_V3_16_DB_V2_1.zip (8.3 MB) 

Precondition

SIZER V3.16 has been installed.

Restriction

If existing SIZER projects with 6FX7... temperature cables are still to be used, data update V2.1 must not be installed as otherwise the system will crash.

This error is corrected with SIZER V3.17.

Workaround

Remove the temperature cables from old projects. Then install data update V2.1.

Installation

  1. Unzip the ZIP file
  2. Double-click the unzipped "SIZER_V3_16_DB_V2_1.szupg" data update package

Content

New products that have been included

  • Addition of PM240-2 frame sizes D - F for the SINAMICS S120 AC drive. Braking resistors cannot be configured. They will follow in the next version.
  • The SINAMICS ET 200SP motor starters have been extended by a 12 A motor starter version.
  • SINAMICS G120C frame sizes D to F
  • New addition of further SINAMICS S120 DC/AC Cabinet Modules.
  • Further SINAMICS G120P devices are added with this update.
  • SIMOTICS S-1FT7, SH132, forced ventilation.
  • CNC option P72.
  • SINUMERIK MCP 416 USB incl. accessories, accessories for MCP 310 USB and MCP 483 USB.
  • New addition of SIMATIC S7-1500 CPU 1511TF-1 PN and SIMATIC S7-1500 CPU 1515TF-2 PN.

Data updates

  • Discontinued signal cables (6FX7...) for temperature sensors updated.
  • Some Motor Modules have been removed due to the phase-out of the SINAMICS S120 Booksize Motor Modules 3 A to 30 A internal cooling.
  • The maximum pre-charging limits for 500 V have been updated for the Line Modules SINAMICS 6SL3330-1TE41-8AA3 and SINAMICS 6SL3330-1TG41-8AA3.
  • SINAMICS G120 devices updated.
  • SINAMICS G120P devices updated and adapted to the current version.
  • The article numbers 6SL3225-0BE25-5AA1, 6SL3225-0BE27-5AA1, 6SL3225-0BE31-1AA1 have been updated for the SINAMICS G120, PM250.
  • SINAMICS G110 circuit breaker types.
  • Article number of the CF card updated to FW4.8.
  • Article number of the IOP Handheld Kit corrected.
  • MicroMaster MM4 circuit breaker types.
  • MicroMaster MM4 Profibus plug connector.
  • SINAMICS PM240, pulse frequency adapted.
  • SINAMICS G120 multicard updated to firmware V4.7 SP6 HF3, Article No. 6SL3054-7TD00-2BA0.
  • Data update so that SIMOTICS GP-1LE1 motors can also be configured for 480 V / 60 Hz (previously 460 V) for operation with converters with an uncontrolled DC link.
  • All SIMOTICS GP/DP-1LA5 motors with shaft heights 180 to 225 in the basic version and IE1 have been removed. Replaced by SIMOTICS GP-1LE1 0/5/6 motors according to the appropriate energy efficiency standard.
  • All remaining SIMOTICS DP/SD 1LA6 motors (shaft heights 100 to 160 in the basic version and IE1) have been removed. Replaced by SIMOTICS GP-1LE150 motors according to the appropriate energy efficiency standard.
  • All remaining SIMOTICS GP-1LA9 motors have been removed. Replaced by SIMOTICS GP-1LE1 0/5/6 motors with energy efficiency standard IE2 or higher.
  • The option texts for SIMOTICS FD motors have been supplemented by the option descriptions A36 (2 Pt1000 resistance thermometers (4 terminals)) and A37 (6 Pt1000 resistance thermometers (12 terminals)).
  • The option texts for SIMOTICS GP/SD 1LE1 motors have been supplemented by the option descriptions Q35 (1 Pt1000 resistance thermometer (2 terminals)) and Q36 (2 Pt1000 resistance thermometers (4 terminals)).
  • The option texts for SIMOTICS GP/SD VSD10 line motors have been supplemented by the option descriptions Q35 (1 Pt1000 resistance thermometer (2 terminals)) and Q36 (2 Pt1000 resistance thermometers (4 terminals)).
  • The option texts for SIMOTICS GP/SD VSD4000 line motors have been supplemented by the option descriptions Q35 (1 Pt1000 resistance thermometer (2 terminals)) and Q36 (2 Pt1000 resistance thermometers (4 terminals)).
  • Inclusion of Pt1000 motor protection for SIMOTICS GP/SD 1LE1 motors. With this extension, the values K and L can be set at the 15th position of the Article number and therefore Pt1000 selected as motor protection.
  • Inclusion of Pt1000 motor protection for SIMOTICS GP/SD VSD10 line motors. With this extension, the values K and L can be set at the 15th position of the Article number and therefore Pt1000 selected as motor protection.
  • Inclusion of Pt1000 motor protection for SIMOTICS GP/SD VSD4000 line motors. With this extension, the values K and L can be set at the 15th position of the Article number and therefore Pt1000 selected as motor protection.
  • For SIMOTICS S-1FG1 servo geared motors, the 14th position of the Article number has been updated for the torque arm version for the 3-stage bevel gearboxes.
  • As part of the relocation of the production of SIMOTICS GP-1LE1 motors from Bad Neustadt to Mohelnice, the Prolifa series will be discontinued. Within this context, the terminal boxes change and option R76, 6-part terminal board, no longer exists.
  • CNC options for SINUMERIK 828D.
  • HT8 device article numbers updated.

Functional improvements

  • The maximum lengths when using motor reactors has been corrected for SINAMICS S120 Motor Module, C/D types.
  • The cabinet widths have been corrected for various SINAMICS S120 DC/AC cabinet units.
  • Maximum cable lengths corrected for SLM.
  • Line reactor for BLM 20 kW corrected.
  • SINAMICS S120 Combi - max. current for the spindle power unit 24 A has been changed from 48 A to 60 A.
  • SIMOTICS S-1FT7062-1(1/5)AF7.- characteristic has been corrected.
  • Corrected data for SIMOGEAR 2KJ3.
  • For SIMOTICS S-1FG1 servo geared motors, SH80 and SH100, the braking torque has been corrected for option N24 (increased braking torque).
  • Missing texts added for CNC options.
  • Article numbers of CNC options have been corrected.
  • Max. number of axes for SINUMERIK 828D has been corrected.
  • CNC options for SINUMERIK 840Dsl.


SIZER for Siemens Drives V3.15

Here you can find version V3.15 of the SIZER engineering tool for drive systems (SINAMICS, MICROMASTER, DYNAVERT T and SIMATIC ET 200 FC), motor starters and control systems (SINUMERIK, SIMOTION and SIMATIC Technology).

Third-party software licensing conditions and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the Readme_OSS.pdf file.

Special note for resellers

The information and the license conditions in the Readme_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
  Readme_OSS.htm (2.5 MB)

 SIZER for Siemens Drives V3.15
 SIZER for Siemens Drives V3.15

  SIZER_V3_15.zip (692.9 MB) 

Optional dimension drawing generator
 Registrierung notwendig  SIZER_V3_15_CAD.zip (135.7 MB)

SIZER can be used free of charge. A nominal order processing fee is charged for the DVD. The software can be used without entering a license key. However, for legal licensing reasons, you should be in possession of a SIZER license certificate (any version). If you do not have a license, you can also order the current SIZER version including the license certificate on a DVD. Article number: 6SL3070-0AA00-0AG0

The readme file contains important information on how to use the tool.

The following installation versions are available

  • Installing SIZER without dimension drawing generators
    • To do this, download the "SIZER_V3_15.zip" file, unpack it, and then start the setup.exe program.
      Important note: The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup.
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
  • Download the "SIZER_V3_15.zip" and "SIZER_V3_15_CAD.zip" and unzip them into a common directory.
  • Start the setup.exe program in the uppermost directory.
    Note:
    A subsequent installation of the dimension drawing generators is also supported via this process.

Important information

The CAD Creator is not part of the scope of delivery of SIZER for Siemens Drives V3.15. To use the CAD functionality, the CAD Creator (as of V1.7.1) must be installed on the PC. You can download the CAD Creator and obtain information about it at 57218443


SIZER for Siemens Drives V3.6

Minimum system requirements

  • PG or PC, Pentium™ III min. 800 MHz (recommended > 1 GHz) 512 MB RAM (recommended > 1 GB)
  • At least 2 GB free hard disk space.
  • Additional 100 MB free hard disk space on the Windows system drive
  • Monitor resolution, 1024x768 pixels
  • Windows 7 32/64 bit (Professional, Enterprise, Ultimate)
  • Windows XP (32/64 bit) Professional, Home Service Pack 2
  • Microsoft Vista Business
  • Microsoft Office 2003/2007/2010

  • Microsoft Internet Explorer 5.5 SP2,
  • MDAC V2.81 SP1

Here you can find version V3.6 of the SIZER engineering tool for drive systems (SINAMICS, MICROMASTER, DYNAVERT T and SIMATIC ET 200 FC), motor starters and control systems (SINUMERIK, SIMOTION and SIMATIC Technology). 

SIZER for Siemens Drives V3.6

SIZER for Siemens Drives V3.6

  sizer_v36.zip (850.1 MB)

Optional dimension drawing generator:

 Registrierung notwendig  sizer_v36_cad.zip (191.4 MB)

SIZER can be used free of charge. A nominal order processing fee is charged for the DVD. The software can be used without entering a license key. However, for legal licensing reasons, you should be in possession of a SIZER license certificate (any version). If you do not have a license, you can also order the current SIZER version including the license certificate on a DVD. Article number: 6SL3070-0AA00-0AG0

The readme file contains important information on how to use the tool.

More information can be found at 54762659

The following installation versions are available


  • Installing SIZER without dimension drawing generators
    • To do this, download the "SIZER_V36.zip" file, unpack it, and then start the setup.exe program.
      Important note: The dimension drawing generators must be deactivated via the "Adapted" setting on the "Setup type" dialog page in the setup. 
  • Installing SIZER with the CAD Generator dimension drawing generator (for standard induction motors)
    • Download the "SIZER_V36.zip" file first and unzip it.
    • Then download the "SIZER_V36_CAD.zip" file. This zip file contains the "Data2.cab" file. This file must be copied or unpacked into the ...\SIZER subdirectory created after unpacking the "SIZER_V36.zip" file. The "Data2.cab" file must then be in the same directory as the "Data1.cab" file. The preselection of the dimension drawing generators is preset in the setup.
    • Start the setup.exe program in the uppermost directory.
      Note: A subsequent installation of the dimension drawing generators is also supported via this process.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.