×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 55111972, Entry date: 08/07/2014
(0)
Rate

Which slot do you have to configure when using the WinAC RTX 2010 with WinCC (TIA Portal)?

  • Entry
  • Associated product(s)

Validity
This entry is valid only if you have the products below installed together on a Windows-based PC system:

  • WinAC RTX 2010
  • WinCC (TIA Portal)

Description
The WinAC RTX 2010 must be configured on slot 2 in the hardware editor of WinCC (TIA Portal) and in the component configuration editor of the Runtime system.

Note
The WinAC RTX 2010 is already configured on slot 2 if the WinAC RTX 2010 is pre-installed as part of a software package.

Keywords
Slot, Panel PC, Panel PC, IPC, Runtime, Advanced,  Professional, Rack PC, Box PC

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.