×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 55394146, Entry date: 10/22/2014
(2)
Rate

How do I configure a VPN tunnel between PC station and Siemens Remote Service Platform via a safety connection?

  • Entry
  • Associated product(s)

Overview
SSL VPN Client creates a tunneled IP-connection between a remote-system (with the SSL-VPNClient) and the Siemens Remote Service Platform.
The SSL VPN Client communicates directly through the internet with the server systems.
This solution requires no additional routers or firewalls, a DSL line is absolutely sufficient.
This tunnel can be used by all TCP/IP based tools. In case of Remote Desktop Support we can use NetMeeting or VNC software.

SSL VPN Client

 

The IPSec VPN termination is realized on the serviced system. In this case the SSL VPN Client on the serviced system is the end-point of this connection.
The connection will be established from the SSL VPN client to the Siemens Remote Service platform.

Requirements  

  • Internet access to a local area network

  • Port 443 from serviced system to the Internet has to be opened

Titel of Downloads Download
Documentation
Siemens Remote Service SSL VPN Client
( 1237 KB )  

Additional Keywords
Siemens Remote Support, VNC, UltraVNC, TightVNC, RealVNC, cRSP, Remote Services, Remote diagnostics, telediagnostics

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.