What options do you have for displaying and editing archives (WinCC Runtime Professional and WinCC V7 Runtime)?
-
Entry
-
Associated product(s)
Configuration Notes
The following table gives an overview of the options for displaying and editing archives in WinCC Runtime.
Note
- All the configuration tools listed here (WinCC functions or options) provide read access to the archive data.
- "w" write access
If the "w" column of a configuration tool has a cross in it, this indicates that this tool supports write access to the archive data. - "csv" option to export data as a text file
If the "csv" column of a configuration tool has a cross in it, this indicates that this tool supports data export in test format (CSV file, for example).
Configuration tool | w | csv | Description |
---|---|---|---|
Process pictures | The following controls are used to display runtime data directly in the WinCC screen. There you also have the possibility to print the data or to export it as a CSV file using the "Export data" function: | ||
x | Alarm View / AlarmControl Further information about this is available in the corresponding manual, for example: | ||
x | f(t) trend display / OnlineTrendControl Further information about this is available in the corresponding manual, for example: | ||
x | Table Display / OnlineTableControl Further information about this is available in the corresponding manual, for example: | ||
x | x | Recipe Display / UserArchiveControl
Further information about this is available in the corresponding manual: | |
Logs | With the "Logs" or "Report Designer" function you can create reports and logs which can be used to clearly print tag and alarm logging data in Runtime Note Detailed information about this is available in the corresponding manual, for example: | ||
Logging Object (VBS) | Using the "Logging Object" you can reconnect swapped-out archive segments to the Runtime or disconnect previously swapped-in archive segments. Further information about "Logging Object" is available in the corresponding manual, for example: | ||
Runtime API | x | x | In WinCC Professional, the option "WinCC/Runtime API" describes the open programming interface of WinCC (Application Programming Interface). Via the API functions, you use the internal functions of WinCC in your own applications and access data from HMI variables or archive data. More information is available here: WinCC Professional V17: Programming Reference > Runtime API With WinCC V7, the "Runtime API" is part of the additionally orderable option WinCC/Open Development Kit (ODK), for example: Technical Data SIMATIC WinCC/ODK V7.5 SP2 |
OLE DB | Using the option "WinCC/Connectivity Pack" you have licensed access to WinCC databases via OPC or WinCC OLE DB provider. Within the TIA Portal, the WinCC OLE DB Provider (W.OLEDB) provides the functionality of the WinCC Connectivity Pack and is integrated into the basic software in WinCC Professional. Further information about the functions of this option is available here: | ||
Industrial Data Bridge | x | x | The option "WinCC/Industrial Data Bridge" provides read and write access to recipes/user archives. Furthermore, it enables the analysis and storage of process values in Office formats and data exchange also with other applications, for example via CSV or XML files. More information about this is available in the application example entitled WinCC/IndustrialDataBridge: Writing data from SIMATIC WinCC or from SIMATIC controllers to Office files |
DataMonitor | x | With the option "WinCC/DataMonitor" you can display and evaluate current process statuses and historical data via the intranet/internet. Detailed information is available the corresponding manual, for example: | |
SIMATIC Process Historian | The "SIMATIC Process Historian" option is used to create a central and scalable long-term archive for the entire plant. With this system it is possible to store data across systems and independent of version from any number of SCADA systems in one database. Further information about "Process Historian" is available in these manuals: | ||
SIMATIC Information Server | x | The web-based "SIMATIC Information Server" option provides continuous reporting from manufacturing to management, based on archived data. It is used to call data of the "WinCC Process Historian" and process it for the user. More information about the "SIMATIC Information Server" is available in the Information Server System Manual. Here you should refer also to the entry entitled What should you watch out for when installing SIMATIC Information Server 2014 SP2 when WinCC is already installed? |
- German
- Italian
- Spanish
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Engineering
- Automation Technology Operator control and monitoring systems HMI Software SIMATIC WinCC V7 SIMATIC WinCC V7 Basic-SW
- Automation Technology Operator control and monitoring systems HMI Software SIMATIC WinCC V7 SIMATIC WinCC V7 Basic-SW General
- Automation Technology Operator control and monitoring systems HMI Software SIMATIC WinCC V7 SIMATIC WinCC V7 Basic-SW Tag Logging
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Runtime
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Runtime WinCC Runtime Professional
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry