×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 56098249, Entry date: 03/20/2014
(0)
Rate

Pharma Demo Applications (Video)

  • Entry
  • Associated product(s)
The media system "Pharma Demo Applications" shows the efficient use of SIMATIC PCS 7 and SIMATIC BATCH in the Pharmaceutical and Life Science Industries using the example of the demo applications "Fermentation, "Blood Fractionation" and "Freeze Drying''.

The media system  includes general process information and graphically explains the configuration, the setup as well as individual process steps of the demo applications. It includes the following chapters:

Introduction

  • Life Science Industry
    Information on Life Science Industry
  • Bio API
    Information on biotechnologically produced active pharmaceutical ingredients

Engineering

  • Introduction
    Overview of the engineering templates and standards used
  • ISA S88.01
    Information on plant models according to ISA S88.01 and their realization with SIMATIC PCS 7 and SIMATIC BATCH
  • Basic Control Modules (BCM)
    General information on BCM and their application

Applications

  • Fermentation
    Introduction of the demo application to the fermentation process
  • Blood Fractionation
    Introduction of the demo application to the process of blood fractionation
  • Freeze Drying
    Introduction of the demo application to the process of freeze drying
 
Media system
 
 
Additional keywords
E-Learning, Tutorial, Teaser, Webcast, Multimedia-based demonstration system, MMDS, Film, Screencast, media system

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.