×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 56314851, Entry date: 11/22/2013
(2)
Rate

Which entries are available in the internet concerning migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?

  • Entry
  • Associated product(s)
The table below gives you an overview of the entries concerning migration to STEP 7 and WinCC in the TIA Portal.

Description
In the table you click the corresponding link (Entry ID) to go to the entry concerned.
 

Description Link 
The webcast included in the entry provides information about migrating STEP 7 V5.x projects to STEP 7 Professional (TIA Portal). The following topics are discussed.
  • Overview of the topic of migration
  • Requirements for migration
  • Conditions for the separate STEP 7 components
 What are the requirements for the migration of STEP 7 V5.x projects in STEP 7 (TIA Portal)? 
Description of the requirements to be fulfilled for migrating your project from STEP 7 V5.x to STEP 7 Professional (TIA Portal).What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)? 
Requirements for installing STEP 7 (TIA Portal)What are the requirements for installing STEP 7 (TIA Portal) V15? 
PLC Migration to S7-1500 with STEP 7 (TIA Portal)PLC Migration to S7-1500 with STEP 7 (TIA Portal) 
Recommended programming for S7-1200 and S7-1500 with STEP 7 (TIA Portal)How do you efficiently and effectively program for the S7-1200/S7-1500 in STEP 7 (TIA Portal)? 
Differences in the keyboard operation of versions of STEP 7 Basic (TIA Portal) and STEP 7 V5.5?What are the differences in the keyboard operation of STEP 7 (TIA Portal) and STEP 7 V5.x? 
Licenses needed to upgrade from STEP 7 version (V5.x or TIA Portal) to the current STEP 7 (TIA Portal).Which license do you need to upgrade from STEP 7 version V5.x, V11 ... V14 to the TIA Portal V15? 
Storage location of the standard blocks and instructions in STEP 7 (TIA Portal) and similarly in STEP 7 V5.5 (SIMATIC Manager)Where are the standard blocks and instructions stored in STEP 7 (TIA Portal) and in V5.5 (SIMATIC Manager)? 
Information about the migration of S7-SCL programsWhat should you watch out for when migrating an S7-SCL program in STEP 7 (TIA Portal)? 
The webcast included in the entry shows you how to migrate a WinCC flexible 2008 SP2 project to WinCC (TIA Portal). The following topics are discussed in the webcast:
  • Overview of the topic of migration
  • Requirements for migration
  • Migration procedure
  • Supplementary information
How do you migrate a WinCC flexible 2008 project to WinCC (TIA Portal)? 
Migration of a WinCC flexible 2008 SP3 project in Windows 7 (64-bit) to WinCC (TIA Portal)How do you transfer global libraries from WinCC flexible to WinCC (TIA Portal)? 
Migration of a global library from WinCC flexible to WinCC (TIA Portal)How do you transfer global libraries from WinCC flexible to WinCC (TIA Portal)? 
Migration of project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)? 
Licenses required to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC (TIA Portal).Where can you find information about the upgrade to SIMATIC WinCC V15? 
Download for the migration tool for generating a migration file for importing into the TIA Portal.

Note
If a project to be migrated is not on the same PG/PC on which the TIA Portal is installed, the output project for the migration must first be converted into a compatible format. The download is available for this.

TIA Portal migration tool 
Shared configuration with WinCC (TIA Portal) and STEP 7 V5.xShared configuration with WinCC (TIA Portal) and STEP 7 V5.x (video) 
Migration Guide: Help for migrating from WinCC flexible to WinCC (TIA Portal)Migration Guide; helps you to migrate from WinCC flexible to WinCC (TIA Portal) 
Overview of all topics on HMI migrationMigration of plants to SIMATIC (TIA Portal) - Visualization 


Additional Keywords
Migration, Transfer


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit