Entry type: FAQ, Entry ID: 56348738, Entry date: 12/04/2013
(0)
Rate

How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?

  • Entry
  • Associated product(s)

Description
The documentation included in this entry describes how to connect a SIMATIC MV440 code reader device to a SIMATIC S7-300 using PROFINET IO.
In this example, a CPU315-2PN/DP is used as PROFINET IO controller.

The figure below illustrates this device configuration.


Fig. 01

Documentation

DP_PROFINET_IO_with_MV440_or_MV420_en.pdf ( 3400 KB )

Sample programs
The downloadable "MV4x0_PROFINET_sample_project_V1_0.zip" file provides you with the following sample program including all the necessary components:

  • The "MV4x0_PROFINET_sample_project_V1.0.ap11" project that was created with STEP 7 (TIA Portal)V11 and includes the configuration of a CPU315-2PN/DP as PROFINET IO controller and a SIMATIC MV440 code reader device as PROFINET IO device.
  • Block "FB79_Application[FC1]", which is called in the user program of the CPU.

MV4x0_PROFINET_sample_project_V1_0.zip ( 2031 KB )

Configuration files
The downloadable "ConfigurationFiles.zip" file provides you with the configuration files for the code reader devices below:
 

Code reader device Configuration file
MV440 SR MV440SR_PROFINET.xml
MV440 HR MV440HR_PROFINET.xml
MV440 UR MV440UR_PROFINET.xml
MV420 SR-B MV420SRB_PROFINET.xml
MV420 SR-P MV420SRP_PROFINET.xml

ConfigurationFiles.zip ( 1948 KB )

Creation environment
The screens and downloads in this FAQ were created with STEP 7 (TIA Portal)V11.

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. Further information can be found in Entry ID: 50203404.

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster