×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 56714946, Entry date: 11/22/2011
(0)
Rate

6AG131* SIPLUS extreme: Micro Memory Cards for S7-300 CPUs

  • Entry
  • Associated product(s)

QUESTION:

Which Micro Memory Cards can be in use together with SIPLUS S7-300 CPUs (6AG131*) ?



ANSWER:

For the product spectrum of SIPLUS S7-300 CPUs are no special “SIPLUS extreme MMC“ available.

The SIMATIC Micro Memory Card with the order number 6ES7 953-8L* can too be in use with the whole SIPLUS extreme spectrum.
The allowed temperature range fulfill too the regulations for the SIPLUS extreme spectrum.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.