×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 56897157, Entry date: 05/25/2018
(4)
Rate

How do you do a recovery for PCS 7 systems during running operation?

  • Entry
  • Associated product(s)
This entry shows you a solution for creating a disk image while the system is in operation. It also includes instructions for configuration using the Veritas System Recovery software.

Note
Please, note that we do not give any warranty for the functioning of the procedure described in this entry, nor do we assume any liability for any faults that might arise when using the Veritas software or the software of any other provider.

The Veritas System Recovery software can be procured from the manufacturer at
www.veritas.com

Note
With SIMATIC PCS 7 V8.2 and higher the information about the compatibility of the different versions is available in the Compatibility Tool

Documentation
  PCS 7 System Recovery with Veritas System Recovery (877,3 KB)


Additional Keywords
Image, Hard disk image

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.