STEP 7 Professional 2010 Service Release 2
-
Entry
-
Associated product(s)
The current product DVD of STEP 7 Professional 2010 has been updated with the Service Pack 2 (SP2) of STEP 7 V5.5 and with the latest options of PLCSIM, S7-Graph and S7-SCL. It is now available for delivery. In addition, the SP2 for STEP 7 V5.5 can be downloaded free of charge from the Internet (see entry ID: 57026339).
Customers with a valid Software Update Service agreement for STEP 7 Professional will receive the DVD with the STEP 7 Professional 2010 Service Release 2 and the current DVD with STEP 7 Professional V11 SP2 automatically. Furthermore, the packaging of STEP 7 Professional 2010 has been extended.
Customers without a Software Update Service agreement for STEP 7 Professional can purchase the Trial License with the STEP 7 Professional 2010 Service Release 2 under the order no.: 6ES7810-5CC11-0YA7. Alternatively, you can also install the Service Packs of the individual products on your STEP 7 Professional 2010 software, e.g. the SP2 for STEP 7 V5.5 via DVD or download (see entry ID 57026339 ).
Preconditions for the installation of STEP 7 Professional 2010 Service Release 2:
- STEP 7 Professional 2010
Supported operating systems:
- MS Windows XP Professional SP2 or SP3
- MS Windows Server 2003 R2 SP2 standard edition as workstation
- MS Windows 7 32 Bit Ultimate, Professional and Enterprise (Standard installation),
with or without SP1. However, the Windows XP mode under Windows 7 is not released. - MS Windows 7 64 Bit Ultimate, Professional and Enterprise with or without SP1
- MS Windows Server 2008 R2 (64 Bit), with or without SP1
Important:
- It is not possible to change the operating system if STEP 7 is installed already. Before you change the operating system, you should be sure to uninstall STEP 7 Professional as well as any other installed STEP 7 option packages.
- If you wish to change to Windows 7 64 Bit with STEP 7 Professional, you require STEP 7 Professional 2010 SR2.
It is not sufficient to only install the Service Pack 2 for STEP 7 V5.5. - More information is available from the readme files
- German: Liesmich.pdf
- English: Readme.pdf ( 74 KB )
Important note concerning the operating systems:
- STEP 7 Professional 2010 SR2 requires the Microsoft Internet Explorer version 6.0 or higher for all operating systems.
What’s NEW?
STEP 7 Professional 2010 Service Release 2 is also released for 64-Bit operating systems.
The Service Release 2 of STEP 7 Professional 2010 updates the following included components:
- STEP 7 V5.5 incl. SP2
- S7-PLCSIM V5.4 incl. SP5
- S7-SCL V5.3 incl. SP6
- S7-GRAPH V5.3 incl. SP7
Starting with STEP 7 Professional 2004 and the new licensing concept for STEP 7 Professional, we have been offering a cost-effective Trial License for validation purposes (not for productive use). This DVD enables you to test all the software packages on the DVD for 14 days (from the day of first starting the software). Thereafter, the complete software can be enabled without any further installation for an unlimited period with the Floating License of STEP 7 Professional. Alternatively, you can also enable the above individual software components with their respective Floating Licenses.
The Trial License for STEP 7 Professional replaces the previous Presales Package..
New packaging of STEP 7 Professional
The DVD with the current version of STEP 7 Professional V11 is additionally included with all new orders for a Floating License of STEP 7 Professional. A Combo License Key is also included for this purpose, enabling the parallel operation of STEP 7 Professional 2010 and STEP 7 Professional V11 on one computer.
Ordering information for the STEP 7 Professional 2010 SR2 Trial License
Order Number. |
Product Name |
6ES7810-5CC11-0YA7 | SIMATIC S7, STEP7 PROFESSIONAL 2010 SERVICE RELEASE 2 DATA CARRIER INCL. TRIAL LICENSE |
- German
- Spanish
- French
- Italian
- Chinese
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry