×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 57204635, Entry date: 01/23/2012
(0)
Rate

Which MMC memory card do I need for the Technology CPUs?

  • Entry
  • Associated product(s)

Description
With the Technology CPUs the firmware for the Integrated Technology is stored on the MMC and uploaded at startup.
The additional functions have increased the size of version V4.1.5 of the firmware for the Integrated Technology to something over 4 MB, so that an MMC with 4 MB is no longer adequate (see also Entry ID 23411204 for version V4.2 and higher of the S7 Technology).

Instructions
Use an MMC with 8 MB (6ES7 953-8LP20-0AA0).

Keywords
T-CPU, 315T, 317T, 317TF

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.