×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 57267466, Entry date: 02/21/2012
(10)
Rate

delivery release: Service Pack 3 for SIMATIC WinCC flexible 2008

  • Entry
  • Associated product(s)
Effective immediately, the Service Pack 3 for SIMATIC WinCC flexible 2008 has been released for delivery. With WinCC flexible 2008 Service Pack 3 the installation on the Windows 7 (64Bit) operating system will be supported. Additionally, some functional expansions in the engineering as well as t...

Effective immediately, the Service Pack 3 for SIMATIC WinCC flexible 2008 has been released for delivery.

With WinCC flexible 2008 Service Pack 3 the installation on the Windows 7 (64Bit) operating system will be supported. Additionally, some functional expansions in the engineering as well as the runtime were incorporated. These are among others, new widescreen resolutions for PC Runtime, support of MP377 15" Touch daylight readable and communication with SIMOTION for the MobilePanel 277 F IWLAN V2.

The Service Pack 3 must be installed on engineering systems as well as on runtime systems. All HMI devices need to be upgraded by an operating system update (image update) too.

Inhalt:

1. Delivery release information

2. New Functionality

3. Product information

    3.1. Compatibility with other SIMATIC Products

    3.2. Special Notes

    3.3. New / revised products

4. Ordering data

5. Further information
  

1. Delivery release information

With the delivery release of Service Pack 3, all WinCC flexible 2008 packages will be changed over to the Service Pack 3. The license keys from WinCC flexible 2008, 2008 SP1 and 2008 SP2 can be used without any change for WinCC flexible 2008 SP3 too.

Due to the statutory regulations for export control we are no longer able to provide the service packs for downloading in the Service&Support Portal. Because of this, the delivery of Service Pack 3 will be in the form of a DVD/CD or by Software Update Service only.

Customers with a valid Software Update Service contract (SUS contract) for WinCC flexible 2008 or WinCC V11 Comfort, Advanced and Professional, will receive the Service Pack 3 automatically.

For customers without a SUS contract, we provide the following supply sources: For a nominal fee the installation medium (DVD/CD) for updating WinCC flexible 2008, 2008 SP1 and 2008 SP2 to WinCC flexible 2008 SP3 can be ordered.

Package

Ordernumber

WinCC flexible 2008 Micro
Update 2008, 2008 SP1, 2008 SP2 -> 2008 SP3

6AV6610-0AA51-3CU8

WinCC flexible 2008 Compact/Standard/Advanced
Update 2008, 2008 SP1, 2008 SP2 -> 2008 SP3

6AV6613-0AA51-3CU8

WinCC flexible 2008 Runtime
Update 2008, 2008 SP1, 2008 SP2 -> 2008 SP3

6AV6613-1XA51-3CU8

You will find information about the Service Pack 3 below.
Information about WinCC flexible 2008 is available at the following link (entry ID: 29735640)
Information about WinCC flexible 2008 SP1 is available at the following link (entry ID: 34780187)
Information about WinCC flexible 2008 SP2 is available at the following link (entry ID: 38612975)
  

2. New functionality

Support of the following Operating Systems

Engineering System:

  • Microsoft Windows XP Home with SP3 (WinCC flexible Micro only)
  • Microsoft Windows XP Professional with SP3
  • Microsoft Windows 7 Professional, Ultimate, Enterprise (32/64 Bit)
  • Microsoft Windows 7 SP1 Professional, Ultimate, Enterprise (32/64 Bit)

Runtime System

  • Microsoft Windows XP Professional with SP3
  • Microsoft Windows 7 Professional , Ultimate, Enterprise (32/64 Bit)
  • Microsoft Windows 7 SP1 Professional, Ultimate, Enterprise (32/64 Bit)
  • Microsoft Windows XP Embedded with SP 2 *)
  • Microsoft Windows XP Embedded Standard 2009 *)
  • Microsoft Windows 7 Embedded Standard (32 Bit) *)
  • Microsoft Windows 7 Embedded Standard with SP1 (32 Bit) *)

    *) only for released platforms e.g. Panel PC 477

New widescreen resolutions for PC Runtime

  • 800 x 480, 1280 x 800, 1980 x 1080

Enhancements for Mobile Panels

  • Communication with SIMOTION also for the Mobile Panels 277F IWLAN V2

Support of new devices

  • MP377 15" Touch Daylight Readable

The new functionalities are summarized in the following document:

    German ( 829 KB )
    English ( 883 KB )
  

3. Product information

3.1. Compatibility with other SIMATIC Products

  • SIMATIC STEP 7 V5.4 SP5 (see entry ID: 36184684)
  • SIMATIC STEP 7 V5.5 (see entry ID: 44370501)
  • SIMATIC STEP 7 V5.5 SP1 (see entry ID: 52336355)
  • SIMATIC STEP 7 V5.5 SP2 (see entry ID: 57026032)

  • SIMATIC STEP 7 V11 (see entry ID: 49639088)
  • SIMATIC STEP 7 V11 SP1 (see entry ID: 51774795)
  • SIMATIC STEP 7 V11 SP2 (see entry ID: 56771572)

  • SIMATIC WinCC V11 (see entry ID: 49740133)
  • SIMATIC WinCC V11 SP1 (see entry ID: 51784423)
  • SIMATIC WinCC V11 SP2 (see entry ID: 56899318)

  • SIMATIC NET CD 2008 SP3 (see entry ID: 40862824)
  • SIMATIC NET PC Software 2008 (V7.1 SP4) (see entry ID: 57989792)
  • SIMATIC NET PC Software 2011 (V8.1 SP1) (see entry ID: 57989792)

  • SIMATIC Logon V1.4 SP1 (see entry ID: 26636275)
  • SIMATIC Logon V1.4 SP2 (see entry ID: 36474276)
  • SIMATIC Logon V1.4 SP3 (see entry ID: 44889581)
  • SIMATIC Logon V1.5 (see entry ID: 58675030)

  • SIMATIC WinCC V7.0 (see entry ID: 29501428)
  • SIMATIC WinCC V7.0 SP1 (see entry ID: 34896120)
  • SIMATIC WinCC V7.0 SP2 (see entry ID: 44451711)
  • SIMATIC WinCC V7.0 SP3 (see entry ID: 55987264)

  • SIMOTION SCOUT V4.1 SP5 (see entry ID: 42469145)
  • SIMOTION SCOUT V4.2 SP1 (see entry ID: 50534427)

  • SIMATIC S7 1200 (see entry ID: 38111886)
  • SIMATIC WinAC RTX 2009 (see entry ID: 37689394)
  • SIMATIC WinAC RTX 2010 (see entry ID: 44356710)
  • SIMATIC WinAC MP 2008 (see entry ID: 31929448)

You will find more released components under the following entry ID 64847781

The following packages are currently not available, the release is carried out with a separate information

  • SINUMERIK HMI Configuring Package WinCC flexible
  • SecureOCX for the legal-for-trade display of SIWAREX FTA (see entry ID: 37453235)
     

3.2. Special notes

  • Recently we have received word of some security issues. These will be solved with Service Pack 3.
    With this in mind, we would like to draw your attention to the following information:
    • Confirmation of security information
      • Starting with WinCC flexible 2008 SP3, the software setup requires a confirmation of an additional security information beside the license terms. This shall indicate the need for an overall IT security concept of the entire automation solution.
    • Link to Siemens Security Advisory
    • Industrial Security home page:
    • Operational Guidelines for Industrial Security
    • FAQ entry for disabling the Telnet service on a HMI Panel
    • FAQ entry for configuration of Runtime Loader
  • Installation of WinCC flexible 2008 SP3 on HP Laptop.
    During the test of WinCC flexible 2008 SP3 we have identified incompatibilities with the HP keyboard driver on HP Laptops. To prevent these incompatibilities, the HP keyboard driver or the WinCC flexible Runtime keyboard driver has to be deinstalled before the installation of WinCC flexible 2008 SP3.
    • How to deinstall the keyboard driver is described under the following entry ID 58217334
       
  • ProTool Migration:
    Because of the neccessary changes for the 64 Bit support under Windows 7, the ProTool migration cannot be offered any more with Service Pack 3 for WinCC flexible 2008.
     
  • Additional information:
        Liesmich ( 323 KB )
        Readme ( 316 KB )
     

3.3. New / revised products

Configuration Sets, Introductory Packages, and Starter Packages

With the release of WinCC flexible 2008 Service Pack 3, the configuration sets, introductory packages, and starter packages will be changed over to the version WinCC flexible 2008 Service Pack 3. The order numbers remain unchanged.
  

4. Ordering data

The order numbers for WinCC flexible 2008 SP3 remain unchanged compared to WinCC flexible 2008, 2008 SP1 and 2008 SP2

/cs/pool/xls.gifOrdering Data WinCC flexible 2008 SP3 ( 42 KB )
  

5. Further information

SIMATIC WinCC flexible:
    www.siemens.com/wincc-flexible

SIMATIC HMI Operator Control & Monitoring Systems:
    www.siemens.com/simatic-hmi

Configuration Efficiency with SIMATIC WinCC flexible the interactive presentation:
    http://www.siemens.com/wincc-flexible-easy