Entry type: FAQ, Entry ID: 57775228, Entry date: 04/15/2014
(10)
Rate

Which license do you need to upgrade from STEP 7 version V5.x, V11 or V12 to the TIA Portal V13?

  • Entry
  • Associated product(s)

Description
If you still do not have a version of STEP 7 installed on your computer, you need the full license for STEP 7 Basic V13 or for STEP 7 Professional V13. If you have a version of STEP 7 installed on your PC, you need either the license for the upgrade or for the PowerPack. The table below shows the different licenses needed for a new installation or for updating your version of STEP 7.
 

Case Procedure
1 No version of STEP 7 installed on your computer.
  • For STEP 7 Basic V13 you need the floating license with article number: 6ES7822-0AA03-0YA5
  • For STEP 7 Professional V13 you need the floating license with article number: 6ES7822-1AA03-0YA5

You can also install the trial license for each product:

  • Article no. for the STEP 7 Basic V13 6ES7822-0AA03-0YA7
  • Article no. for the STEP 7 Professional V13 6ES7822-1AA03-0YA7

Note
As registered customer you can download the trial for SIMATIC STEP 7 Professional V13 and test it for 21 days. The Professional edition also includes the functions from SIMATIC STEP 7 Basic V13. More information is available in Entry ID: 78793685.

2 You have STEP 7 Professional 2006 or 2010 installed on your computer and you want to upgrade to STEP 7 Professional V13.
  • Here you need the upgrade with the COMBO floating license (article number: 6ES7822-1AA03-0XE5).
3 You have STEP 7 Basic V11 or V12 installed on your computer and you want to upgrade to STEP 7 Basic V13.
  • Here you need the floating upgrade package license (article number: 6ES7822-0AA03-0YE5).

Note
Valid for STEP 7 V11 Single and for STEP 7 V11 Floating.

4 You have STEP 7 Professional V11 or V12 installed on your computer and you want to upgrade to STEP 7 Professional V13.
  • Here you need the upgrade with the floating license (article number: 6ES7822-1AA03-0YE5).

Note
It is not possible to use this upgrade to upgrade from STEP 7 Professional 2010.

5 You have STEP 7 V5.4 or V5.5 installed on your computer and you want to upgrade to STEP 7 Professional V13.
  • Here you need the PowerPack & Upgrade with the floating license (article number: 6ES7822-1AA03-0XC5).
6 You have STEP 7 Basic V13 installed on your computer and you want to change to STEP 7 Professional V13.
  • Here you need the PowerPack with the floating license (article number: 6ES7822-1AA03-0YC5).
7 You have STEP 7 Professional 2010/V11 or 2010/V12 installed on your computer and you want to upgrade to STEP 7 Professional 2010/V13.
  • Here you need the Combo floating license (article number: 6ES7822-1AA03-0YE5) for SIMATIC STEP 7 PROFESSIONAL V13 ENGINEERING SOFTWARE.
Table 01

The floating licenses are also available here for downloading. Entry 84047138 contains the list with the article numbers at the link "STEP_7_V12_Orderlist". The article numbers are linked with the associated downloads.

The table below shows the features of the different license keys that you can order and install.
 

License Key Meaning
Single License Unlimited use on any one computer.
Floating License Unlimited use on any one computer or through the network.
Rental License Limited use as stipulated in the rental contract.
Trial License Limited use (max. 21 days) for tests and for validating (with disclaimer).
Upgrade License An Upgrade License converts a license for an earlier version x to a license for version >x+... .
Table 02

You can also install STEP 7 V5.5, WinCC flexible 2008 onwards and WinCC V7.0 SP2 onwards in parallel to STEP 7 V13.

  • With an Upgrade License / Combo License for STEP 7 V13 (TIA Portal) you can operate both STEP 7 V5.5 or STEP 7 Professional 2010 and STEP 7 Professional V12.
  • With a Full License for STEP 7 V13 (TIA Portal) you cannot operate STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010.

Follow the instructions in the table below to upgrade a License Key.
 

No. Procedure
1 Open the Automation License Manager and select "View > Management".
2 Transfer the Upgrade License Key to the hard disk on which you want to carry out the upgrade.
3 Also transfer the License Key of the previous version to the hard disk if the license is not yet located on your computer.
4 Select the storage location in the navigation area where the license key to be upgraded is located (previous version).
5 In the Object area you select the license key that is to be upgraded.
6 Execute the menu command "License Key > Upgrade...". The upgrade is now made.


Fig. 01

Table 03

TIA Selection Tool
More information is available in the TIA Selection Tool (http://www.siemens.com/tia-selection-tool). Using the Totally Integrated Automation Selection Tool (TIA Selection Tool) you can select, configure and order devices for Totally Integrated Automation. The TIA Selection Tool provides you with wizards for selecting the required devices, Station Configuration Editors for selecting modules and accessories and for testing proper functioning.

Note
More information about licenses and the differences between the authorizations and licenses is available in Entry ID: 19020864

Creation environment
The screen in this FAQ response was created with ALM V5.3 + Upd 1.

ProductSupport.EntityResultListTitle
ProductSupport.EntityResultListDescription

ProductSupport.EntityResultListButtonText
Copy URL
mySupport Cockpit
Related links