×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 57775348, Entry date: 02/01/2012
(0)
Rate

How can you convert REAL values displayed in the program comparator of SIMATIC S7 F Systems V6.1 to a floating point number?

  • Entry
  • Associated product(s)

Description
In SIMATIC S7 F Systems V6.1 REAL values converted when comparing two safety programs are displayed in hexadecimal format.


Fig. 01: Output of the program comparator in F Systems V6.1

In the versions prior to SIMATIC F-Systems V6.1 and as from version V6.1 SP1 REAL values are displayed in floating point number format.

Instructions
The output format of the values in the program comparator cannot be changed by means of system settings. In order to be able to check the values in the program comparator you must use the program provided in the download specified below. This program converts the HEX numbers into floating point numbers.
 

Description

Download

Application for displaying hexadecimal numbers as floating point numbers.


DTR.zip ( 4 KB )

Creation environment
The screens in this FAQ were created with PCS 7 V7.1 SP3 and F Systems V6.1.

Keywords
Floating point numbers

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit