Entry type: Download, Entry ID: 58112582, Entry date: 10/31/2012
(3)
Rate

Updates for STEP 7 V11 SP2 and WinCC V11 SP2

  • Entry
  • Associated product(s)
   

Update 5

The update is applicable to the following products:

  • STEP 7 Basic/Professional V11.0 SP2
  • WinCC Basic/Comfort/Advanced/Professional V11.0 SP2

Update 5 contains all the changes of Updates 1 to 4.

Improvements over earlier versions:

STEP 7 Basic/Professional

  • Improvements within the framework of Teleservice connections
  • Detailled display of the cross-reference list
  • Stability improvements in the migration of projects
  • Stability improvements in the SCL editor
  • Other stability improvements
     

WinCC Basic/Comfort/Advanced/Professional

  • Engineering System - stability improvements
  • Engineering System - improvements with image objects of the project library
  • Engineering System - improvements with the conversion of a WinCC or STEP 7 project of version 10.5 with images or image objects in the project library
  • Engineering System - improvements with S7 diagnostic messages in projects that were migrated from WinCC flexible
  • KTP600 Basic - improvement of the runtime characteristics
  • TP 177A - improvement of the response when changing the communication parameters
  • OP 73 - improvement of the response after removing and returning the communication cable
  • KP400 Basic color and KTP400 Basic color - improvements when updating the operating system
     

The readme file for Update 5 is available here ( 125 KB ) .

The update is to be installed on the engineering system. For the operator devices, a recompilation and transfer are required to load the update onto the target device.
The latest update for WinCC Runtime Advanced V11 SP2 is available at entry ID 58112587 and the latest update for WinCC Runtime Professional V11 SP2 at entry ID 59539754.

Update 5 can only be installed if one of the products STEP 7 V11.0 SP2 or WinCC V11.0 SP2 is already installed.
To install the update, all 3 files must be downloaded to the same directory; now start SIMATIC_TIAP_V11_0_SP2_UPD5.exe.

Download of Update 5 for STEP 7 Basic/Professional and WinCC Basic/Comfort/Advanced/Professional V11 SP2 

SIMATIC_TIAP_V11_0_SP2_UPD5.exe ( 1799 KB )

SIMATIC_TIAP_V11_0_SP2_UPD5.001 ( 665600 KB )

SIMATIC_TIAP_V11_0_SP2_UPD5.002 ( 665600 KB )

SIMATIC_TIAP_V11_0_SP2_UPD5.003 ( 26813 KB )   


Update 4

The update is applicable to the following products:

  • STEP 7 Basic/Professional V11.0 SP2
  • WinCC Basic/Comfort/Advanced/Professional V11.0 SP2

Update 4 contains all the changes of Updates 1 to 3.

Improvements over earlier versions

STEP 7 Basic/Professional

  • PLC Copy functionality for standard S7-300, S7-400 (Flash Memory), ET200S and ET200Pro CPUs
  • User administration for IM151-8 Web server
  • Stability improvements in the SCL Editor
  • Further stability improvements

WinCC Basic/Comfort/Advanced/Professional

  • Migration
  • Compilation and loading of devices
  • Improvements with control messages
  • Basic Panels: Variables for KTP 1000 Basic PN
  • Mobile Panels: On screen keyboard
  • Sm@rtServer: Login Sm@rtClient
  • Pack & Go

The readme file for Update 4 is available here ( 125 KB )

The update must be installed on the engineering system. For the operator devices, a recompilation and transfer are required to load the update to the target device.
The latest update for WinCC Runtime Advanced V11 SP2 is available at entry ID 58112587 and the latest update for WinCC Runtime Professional V11 SP2 at entry ID 59539754.

Update 4 can only be installed if one of the products is already installed.

Download of Update 4 for STEP 7 Basic/Professional and WinCC Basic/Comfort/Advanced/Professional V11 SP2 

 

SIMATIC_TIAP_V11_0_SP2_UPD4.exe ( 1799 KB )

SIMATIC_TIAP_V11_0_SP2_UPD4.002 ( 665178 KB )

SIMATIC_TIAP_V11_0_SP2_UPD4.001 ( 665600 KB )


Update 3

The update is applicable to the following products:

  • STEP 7 Basic/Professional V11.0 SP2
  • WinCC Basic/Comfort/Advanced/Professional V11.0 SP2

Update 3 contains all the changes of Update 1 and Update 2.

Improvements over earlier versions:

STEP 7 Basic/Professional

  • Support of firmware version 3.0 for S7-1200 controllers
  • Growth of the project size in conjunction with SCL blocks has been eliminated
  • Additional improvements in the migration of STEP 7 V5.x
  • Performance enhancements with online functions
  • The length of commentaries in block interfaces and data blocks is no longer limited
  • Further stability improvements

WinCC Basic/Comfort/Advanced/Professional

  • Migration of WinCC flexible 2008 SP3 projects now possible
  • Improvements with the migration
  • Improvement when compiling and loading devices
  • Screen resolutions of 800x480, 1280x800, 1980x1080 for Runtime Advanced
  • Improved system diagnostic indication on Comfort Panels
  • Improvement with the operating system update on Comfort Panels
  • Improvement of the system functions on panels
  • Cyrillic characters now available on KP300 Basic

Furthermore, Update 3 features improvements in the representation of the installed software.

The readme file for Update 3 is available here .

The update is to be installed on the engineering system. For the operator devices, a recompilation and transfer are required to load the update onto the target device.
The latest update for WinCC Runtime Advanced V11 SP2 is available at entry ID 58112587 and the latest update for WinCC Runtime Professional V11 SP2 at entry ID 59539754.

Update 3 can only be installed if at least one of these products is already installed.

Download of Update 3 for STEP 7 Basic/Professional and WinCC Basic/Comfort/Advanced/Professional V11 SP2 

SIMATIC_TIAP_V11_0_SP2_UPD3.exe ( 1797 KB )

SIMATIC_TIAP_V11_0_SP2_UPD3.002 ( 524222 KB )

SIMATIC_TIAP_V11_0_SP2_UPD3.001 ( 665600 KB )    


Update 2

The update is applicable to the following products:

  • STEP 7 Basic/Professional V11.0 SP2
  • WinCC Basic/Comfort/Advanced/Professional V11.0 SP2

The update includes all changes of Update 1.

Improvements over earlier versions:

STEP 7 Basic/Professional

  • Extensive stability improvements, in particular for SCL and online functionality 
  • Improved migration from STEP 7 V5.x
  • Hardware configuration:
    • Stability improvements for ASi configuration

If, contrary to expectations, problems still occur when working with existing SCL projects or library elements (even after Update 2 has been installed), please contact your Siemens representative or the customer support.

WinCC Basic/Comfort/Advanced/Professional

Update 2 includes all changes of Update 1.
In addition, Update 2 comes with the following improvements:

  • Improved system stability 
  • Improvements with regard to "Find and Replace" and the cross-device copying of screens
  • Improvements when compiling panels 
  • Improvements when compiling Runtime Professional
  • Improved system diagnostics with regard to the display on Comfort Panels
  • Indicator LEDs for panels with softkeys
  • Exiting of Runtime on Comfort Panels

The update is to be installed on the engineering system. For the operator devices, a recompilation and transfer are required to load the update onto the target device.
Update for WinCC Runtime Advanced V11 SP2 at entry ID 58112587, Update for WinCC Runtime Professional V11 SP2 at entry ID 59539754

Update 2 can only be installed if at least one of these products is already installed.

Download of Update 2 for STEP 7 Basic/Professional and WinCC Basic/Comfort/Advanced/Professional V11 SP2 

SIMATIC_TIAP_V11_0_SP2_UPD2.exe ( 1797 KB )

SIMATIC_TIAP_V11_0_SP2_UPD2.001 ( 665600 KB )

SIMATIC_TIAP_V11_0_SP2_UPD2.002 ( 472573 KB )

 


Update 1

The update is applicable to the following products:

  • WinCC Basic/Comfort/Advanced/Professional V11 SP2

Improvements over earlier versions:

In the recent past, a number of security vulnerabilities have been reported, which are remedied with Update 1 for V11 SP2.
In this context, we would like to point out the following information:

In addition, Update 1 includes adjustments to the scripting for faceplates on Runtime Professional devices.

The update is to be installed on the engineering system. For the operator devices, a recompilation and transfer are required to load the update onto the target device.

Update for WinCC Runtime Advanced V11 SP2 58112587

Update 1 can only be installed if at least one of these products is already installed.

Download of Update 1 for WinCC Basic/Comfort/Advanced/Professional V11 SP2 

SIMATIC_TIAP_V11_0_SP2_UPD1.exe ( 8901 KB )