×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 58364219, Entry date: 02/01/2012
(1)
Rate

Release of Automation License Manager (ALM) V5.1 SP1 Update 3 for powermanager

  • Entry
  • Associated product(s)

The latest version of the Automation License Manager (ALM) V5.1 SP1 Update 3 is now released for powermanager V2.0 and V3.0.

Other content:

Since December there is an update of the Automation License Manager (ALM) available that fixes a secutity issue. This Version is V5.1 SP1 Update 3.

This version of the Automation License Manager (ALM) is also released for powermanager V2.0 and V3.0.

The update can be downloaded at the following link:

Entry ID: 114358

Due to the fact that the ALM V5.1 SP1 Update 3 is not released for the OS Microsoft VISTA, an installation of this ALM version in combination with VISTA and powermanager V2.0 is not released either.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.