×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 584459, Entry date: 01/24/2019
(4)
Rate

Which modules support the "S7 Routing" function in S7 subnets?

  • Entry
  • Associated product(s)
This entry shows which modules support the "S7 Routing" function in S7 subnets to be able to operate cross-network PG/OP communication through S7 Routing.

S7 Routing in S7 subnets is possible via Ethernet, PROFIBUS and MPI subnets. With the PG/PC you can reach devices beyond subnet limits to do the following, for example:

  • Download user programs
  • Download hardware configurations
  • Run test and diagnostic functions

Example for S7 Routing
The figure below shows the access from a PG to PROFIBUS via Ethernet.


Fig. 01

Requirements for S7 Routing

  • The CPUs, CMs and CPs support the "S7 Routing" function.
  • All the devices using the gateway must receive information about which subnets can be reached via which routes (= routing information). The devices receive the routing information through downloading the hardware configuration in the CPUs.
    In the case of a topology with several subnets you must keep to the following order when downloading: First you download the hardware configuration into the CPU(s), which are connected to the same subnet as the PG/PC; then you download the CPUs of the other subnets one after the other starting with the nearest subnet through to the most distant.
  • The PG/PC with which you wish to set up a connection via a gateway must be assigned to the subnet to which it is physically connected.
  • For PROFIBUS subnets: The CPU must either be configured as a DP master or if it is configured as DP slave, the check box "Test, commissioning and routing" must be checked in the Properties of the DP interface of the DP slave.
  • For S7-1500 CPUs: At the second interface you must configure a PN/IE subnet so that the CPU recognizes that "S7 Routing" is to be executed.

SIMATIC S7 CPUs
The list below gives an overview of the SIMATIC S7 CPUs which support the "S7 Routing" function.

  584459_overview_cpus_en.pdf (102,1 KB)

Communication processors (CPs)
The list below gives an overview of the PROFIBUS and Industrial Ethernet CPs which support the "S7 Routing" function.

  584459_overview_cps_en.pdf (122,9 KB)

SIMATIC S7 FM modules
The list below gives an overview of the SIMATIC S7 FM modules which support the "S7 Routing" function.
 

FM

Version

Article number

FM 356-4V5.0 V5.0 6ES7356-4BM00-0AE0
FM 356-4V5.0 V5.0 6ES7356-4BN00-0AE0
FM 456-2 V5.0 6ES7456-2AA00-0AB0
Table 01

Gateways
The list below gives an overview of the gateways which support the S7 Routing function.
 

Link

Version

Article number

IE/PB Link V1.0 and higher 6GK1411-5AA00
IE/PB Link PNIO V1.0 and higher 6GK1411-5AB00
IWLAN/PB Link PNIO V1.1 and higher 6GK1417-5AB00
IWLAN/PB Link PNIO V1.1 and higher 6GK1417-5AB01
Table 02

SIMATIC S7 IM modules
The list below gives an overview of the SIMATIC S7 IM modules which support the S7 Routing function.
 

IM

Version

Article number

IM 467 V2.0 and higher 6ES7467-5GJ02-0AB0
IM 467-FO V2.0 and higher 6ES7467-5FJ00-0AB0
Table 03

SIMATIC WinAC RTX, WinAC Slot and WinAC MP
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP which support the S7 Routing function.

WinAC Version Article number
WinAC RTX V4.0 and higher 6ES7671-0R...
WinAC Slot 412 V3.2 and higher 6ES7673-2C...
WinAC Slot 416 V3.2 and higher 6ES7673-6C...
WinAC MP V4.1 and higher 6ES7671-4EE00-0YA0
6ES7671-5EF01-0YA0
6ES7671-7EG01-0YA0
Table 04

SINAUT communication modules
The list below gives an overview of the SINAUT communication modules which support the S7 Routing function.
 

TIMVersionArticle number
TIM 1531 IRC
V1.0 and higher6GK7543-1MX00-0XE0
TIM 3V-IEV1.0 and higher6NH7800-3BA00
TIM 3V-IE AdvancedV1.1 and higher6NH7800-3CA00
TIM 4R-IEV1.0 and higher6NH7800-4BA00
TIM 4RDV3.x and higher6NH7800-4AD90
Table 05

Note

  • If you send data from an Engineering Station that is connected to PROFINET to field devices via PROFIBUS, then you use the "Data record routing" function. Further information about the "Data record routing" function is available in Entry ID 7000978.
  • The target station does not have to support the S7 Routing function. The Basic Panels are the exception here. The Basic Panels cannot be a routing destination.

Further Information

Entry 109474569gives instructions for making an S7 station configured in STEP 7 V5.x routing-compatible for an S7 station configured in the TIA Portal.

Additional Keywords
Module function

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit