×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 58522603, Entry date: 02/05/2015
(12)
Rate

How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?

  • Entry
  • Associated product(s)

Description
The document below informs you how to transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet.

Contents

1.Transfer from a Configuration Computer with Windows 7 using Ethernet
    1.1 Instructions
    1.2 Settings on the Operator Panel
    1.3 Settings on the Configuration Computer
    1.4 Checking the Ethernet Connection
        1.4.1 Checking the Connection to the Panel
        1.4.2 Checking the Settings on the Operator Panel
    1.5 Settings in WinCC (TIA Portal)

Download
WinCC_TIA_Portal_Ethernet_Transfer_en.pdf ( 758 KB )

Security information
Siemens provides products and solutions with industrial security functions that support the secure operation of plants, solutions, machines, equipment and/or networks. They are important components in a holistic industrial security concept. With this in mind, Siemens’ products and solutions undergo continuous development. Siemens recommends strongly that you regularly check for product updates.
For the secure operation of Siemens products and solutions, it is necessary to take suitable preventive action (e.g. cell protection concept) and integrate each component into a holistic, state-of-the-art industrial security concept. Third-party products that may be in use should also be considered. For more information about industrial security, visit
http://www.siemens.com/industrialsecurity.
To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Additional Keywords
Download, Transfer, Load, Control Panel, Channel, Remote Control, Commissioning, Project transfer, Bus address, Transmission rate, Nodes, Stations

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.