×
Siemens Industry Online Support
Siemens AG
文档类型 软件下载 文档编号 58638200, 文档发布日期 2021年7月13日
(56)
评估

Migration Tool TIA Portal

  • 文档
  • 涉及产品
Description, procedure and download of the Migration Tool TIA Portal (V13 SP2, V14 SP1, V15, V15.1, V16)

Description

In many cases, a project that you want to migrate is not on the same programming device / PC as the one on which the TIA Portal is installed. The original project must therefore first be converted to a compatible format for the migration. Then copy the migration file to the programming device or PC with the latest installation of the TIA Portal. There, you can then import the file into the TIA Portal and create a project in the current file format of the TIA Portal.

Procedure

To perform migration without the original software, you need to take the following steps:

  • Install the Migration Tool on the programming device / PC with the source project.
  • Start the Migration Tool and use it to convert the source project into the migration file format with the corresponding file extension ".amxx".
  • When performing this step, ensure that the complete software required for processing the source project is installed on the programming device / PC. This includes all required service packs, hardware support packages and all the add-on software necessary for processing the original project. If some products are not installed, the migration cannot be performed or can only be partially performed.
  • Copy the migration file to the destination system with the most recent installation of the TIA Portal.
  • Note that all required TIA Portal products, which are necessary for configuring all devices contained in the migration file, must be installed on the target system.
  • Perform the migration within the TIA Portal and specify the migration file as the source.
  • Check the log file following the migration and systematically work through any remarks in the newly created project. Also pay special attention to the remarks in the Inspector window after the initial compiling of the configuration.

Supported software products

The Migration Tool supports the migration of the following projects (as of version):

  • STEP 7 Professional 2010
  • STEP 7 V5.5
  • WinCC V7.2
  • WinCC flexible 2008 SP2 / SP3 / SP5
  • Distributed Safety V5.4
     

Download Migration Tool

  • The Migration Tool is located on every STEP7 Prof / WinCC Comfort / WinCC Adv. or WinCC Prof. DVD in the following foldern:
    Support/SIMATIC_Migration_Tool_TIA_Vxxxx.exe

  • Alternatively, you can download the Migration Tool directly:


Migration tool V17:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V17.iso (231.7 MB)

SHA-256 checksum for Migration Tool V17:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V17.txt (1 KB) Information on SHA-256


Migration tool V16:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V16_Upd4.exe (158.2 MB)

SHA-256 checksum for Migration Tool V16:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V16_Upd4.txt (1 KB) Information on SHA-256


Migration tool V15.1:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_1_Upd6.exe (150.4 MB)

SHA-256 checksum for Migration Tool V15.1:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_1_Upd6.txt (1 KB) Information on SHA-256


Migration tool V15:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_Upd4.exe (148.3 MB)

SHA-256 checksum for Migration Tool V15:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_Upd4.txt (1 KB) Information on SHA-256


Migration Tool V14 SP1*:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.exe (147.2 MB)

SHA-256 checksum for Migration Tool V14 SP1:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.txt (1 KB) Information on SHA-256

Compared to the Migration Tool on the STEP7 / WinCC DVD, the file "SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.exe" also supports Windows 7 32-bit operating systems and the migration of WinCC flexible 2008 SP5 projects.


Migration Tool V13 SP2*:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.exe (119.5 MB)

SHA-256 checksum for Migration Tool V13 SP2:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.txt (1 KB) Information on SHA-256

* 09/2017: Compared to the Migration Tool on the STEP7 / WinCC DVD, the file "SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.exe" supports the migration of WinCC flexible 2008 SP5 projects.


Download Safety Plug-in for the Migration Tool

  • The Safety Plug-in for the Migration Tool is located on every STEP7 Safety DVD in the following folder:
    Support/Safety_PlugIn_Migration_Tool_TIA_Vxxxx.exe
  • Alternatively, you can download the plug-in directly:

Safety V13 SP2:

 Download unterliegt Exportcontrolle  Safety_PlugIn_Migration_Tool_TIA_V13_SP2.exe (15.1 MB)

Safety V14 SP1:

 Download unterliegt Exportcontrolle  Safety_PlugIn_Migration_Tool_TIA_V14_SP1.exe (16.3 MB)




安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。