×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 58638200, Entry date: 12/06/2019
(46)
Rate

Migration Tool TIA Portal

  • Entry
  • Associated product(s)
Description, Procedure and Download Migration Tool ( V13 SP2, V14 SP1, V15, V15.1 )

Description

In many cases, a project that you want to migrate is not on the same programming device / PC as the one on which the TIA Portal is installed. The original project must therefore first be converted to a compatible format for the migration. Then copy the migration file to the programming device or PC with the latest installation of the TIA Portal. There, you can then import the file into the TIA Portal and create a project in the current file format of the TIA Portal.

Procedure

To perform migration without the original software, you need to take the following steps:

  • Install the Migration Tool on the programming device / PC with the source project.
  • Start the Migration Tool and use it to convert the source project into the migration file format with the corresponding file extension ".amxx".
  • When performing this step, ensure that the complete software required for processing the source project is installed on the programming device / PC. This includes all required service packs, hardware support packages and all the add-on software necessary for processing the original project. If some products are not installed, the migration cannot be performed or can only be partially performed.
  • Copy the migration file to the destination system with the most recent installation of the TIA Portal.
  • Note that all TIA Products required for configuring all the devices listed in the migration file must be installed on the destination system.
  • Perform the migration within the TIA Portal and specify the migration file as the source.
  • Check the log file following the migration and systematically work through any remarks in the newly created project. Also pay special attention to the remarks in the Inspector window after the initial compiling of the configuration.

Supported software products

The Migration Tool supports the migration of the following projects (as of version):

  • STEP 7 Professional 2010
  • STEP 7 V5.5
  • WinCC V7.2
  • WinCC flexible 2008 SP2 / SP3 / SP5
  • Distributed Safety V5.4

Download Migration Tool

  • The Migration Tool is located on every STEP7 Prof / WinCC Comfort / WinCC Adv. or WinCC Prof. DVD in the following folder:
    Support/SIMATIC_Migration_Tool_TIA_Vxxxx.exe

  • Alternatively, you can download the Migration Tool directly:

Migration Tool V13 SP2*:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.exe (119,5 MB)

SHA-256 Checksum for Migration Tool V13 SP2:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.txt (1 KB) Information on SHA-256

* 09/2017: Compared to the Migration Tool on the STEP7 / WinCC DVD, the file "SIMATIC_Migration_Tool_TIA_V13_SP2_Upd1.exe" also supports the migration of WinCC flexible 2008 SP5 projects.


Migration Tool V14 SP1*:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.exe (147,2 MB) 

SHA-256 Checksum for Migration Tool V14 SP1:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.txt (1 KB)    Information on SHA-256

*Compared to the Migration Tool on the STEP7 / WinCC DVD, the file "SIMATIC_Migration_Tool_TIA_V14_SP1_Upd7.exe" also supports Windows 7 32-bit operating systems and  the migration of WinCC flexible 2008 SP5 projects.


Migration Tool V15:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_Upd4.exe (148,3 MB)

SHA-256 Checksum for Migration Tool V15

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_Upd4.txt (1 KB)Information on SHA-256


Migration Tool V15.1:

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_1_Upd4.exe (148,7 MB)

SHA-256 Checksum for Migration Tool V15.1

 Registrierung notwendig  SIMATIC_Migration_Tool_TIA_V15_1_Upd4.txt (1 KB) Information on SHA-256 


Download Safety Plug-in for the Migration Tool

  • The Safety Plug-in for the Migration Tool is located on every STEP7 Safety DVD in the following folder:
    Support/Safety_PlugIn_Migration_Tool_TIA_Vxxxx.exe
  • Alternatively, you can download the plug-in directly:

Safety V13 SP2:

Download unterliegt Exportcontrolle Safety_PlugIn_Migration_Tool_TIA_V13_SP2.exe (15.1 MB)

Safety V14 SP1:

Download unterliegt Exportcontrolle Safety_PlugIn_Migration_Tool_TIA_V14_SP1.exe (16.3 MB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.