×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 58638618, Entry date: 02/15/2012
(0)
Rate

CEMAT V7.1+SP1 with CEMAT Hotfix dated Jan. 27, 2012 released for SIMATIC PCS 7 V8.0

  • Entry
  • Associated product(s)

CEMAT V7.1+SP1 is herewith released for operation with SIMATIC PCS 7 V8.0 after installation of the CEMAT Hotfix dated Jan. 27, 2012. Please keep in mind that SIMATIC PCS 7 V8.0 must always be installed first, then CEMAT V7.1+SP1 and finally the CEMAT Hotfix. Beyond that, no other restrictions exist.

When you modify or newly create CEMAT projects, please also read the information on updating the SIMATIC PCS 7 V6.x or V7.x software to V8.0 in the manual "SIMATIC PCS 7 V8.0 - Software updating without use of the new functions".

The CEMAT Hotfix dated Jan. 27, 2012 is not yet included with new shipments of CEMAT V7.1+SP1. It is provided for download at entry ID 58638405.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.