×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 58703073, Entry date: 10/18/2012
(6)
Rate

SINAMICS S: Positioning of a S110 using S7-300/400 (STEP 7 V5) with PROFINET/PROFIBUS and Safety Integrated (via PROFIsafe and fail-safe inputs)

  • Entry
  • Associated product(s)

Task
The SINAMICS S110 is to be controlled via a fieldbus (PROFINET/PROFIBUS) from an S7-300 CPU in order to be able to change the traversing blocks from the controller. This option is also to apply for safety functions.

Solution
The function block FB 283 is used for this purpose in this application example. FB 283 controls the cyclic communication and provides various types of acyclic jobs, such as:

  • A function to read and write the traversing blocks.
  • A user-friendly option to change or read arbitrary parameters.

If you want to use the S110 safety functions, information on setting up the functions can be found in the appropriate section in the documentation. Extended safety functions are also available. These require a license and are not considered in this application example. For PROFIsafe a F-CPU is needed.

This application example shows a possible solution for your task. You can use this as a stimulation or basis for your own solutions.

Advantage
This application example provides the following advantages:

  • Uniform data transfer between the SIMATIC controller and the SINAMICS drive
  • Even large data volumes can be clearly arranged with the standard features of the SIMATIC CPU (User-Defined Types / UDTs)
  • Use of safety functions via the same standard bus (PROFINET/PROFIBUS)

Benefits
You can react more flexibly to your individual requirements and save time thanks to the interaction between the SIMATIC CPU and the SINAMICS drive.

Downloads

Content of downloads PROFINET

PROFIBUS

Positioning of a S110 with S7-300 via PROFINET/PROFIBUS in STEP 7 with Safety Integrated via PROFIsafe Documentation 58703073_FE_FB283_Profinet_Profisafe_en.pdf ( 1283 KB ) 58703073_FE_FB283_Profibus_Profisafe_en.pdf ( 1076 KB )
Code
S7-Projekt
58703073_Profinet_Profisafe.zip ( 644 KB ) 58703073_Profibus_Profisafe.zip ( 635 KB )
Safety Evaluation Tool Projekt IEC
The Safety Evaluation Project can only be opened with the Safety Evaluation Tool.
58703073_IEC_Profinet_Profisafe_en.zip ( 7 KB ) 58703073_IEC_Profibus_Profisafe_en.zip ( 7 KB )
Safety Evaluation Tool Projekt ISO
The Safety Evaluation Project can only be opened with the Safety Evaluation Tool.
58703073_ISO_Profinet_Profisafe_en.zip ( 7 KB ) 58703073_ISO_Profibus_Profisafe_en.zip ( 7 KB )
Positioning of a S110 with S7-300 via PROFINET/PROFIBUS in STEP 7 with Safety Integrated via terminal Dokumentation FE_FB283_Profinet_en.pdf ( 1143 KB ) 58703073_F-DI_FE_FB283_Profibus_en.pdf ( 1006 KB )
Code
S7-Projekt
58703073_Profinet.zip ( 540 KB ) 58703073_F-DI_Profibus.zip ( 546 KB )
Safety Evaluation Tool Projekt IEC
The Safety Evaluation Project can only be opened with the Safety Evaluation Tool.
58703073_IEC_Profinet_en.zip ( 3 KB ) 58703073_F-DI_IEC_Profibus_en.zip ( 3 KB )
Safety Evaluation Tool Projekt ISO
The Safety Evaluation Project can only be opened with the Safety Evaluation Tool.
58703073_ISO_Profinet_en.zip ( 3 KB ) 58703073_F-DI_ISO_Profibus_en.zip ( 3 KB )
Link to the Safety Evaluation Tool
www.siemens.com/safety-evaluation-tool

Note on security
Caution
The functions and solutions described in this article confine themselves to the realization of the automation task predominantly. Please take into account furthermore that corresponding protective measures have to be taken up in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the Internet. Further information can be found under the Item-ID 50203404.

Last change
First edition

Additional search terms
motioncontrol_apc_applications