×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 58804919, Entry date: 02/20/2017
(5)
Rate

Safety Laser Scanner with Monitoring Case Switching on an S7-1500

  • Entry
  • Associated product(s)
An assembly cell with a robot has two workstations that can alternately be freely accessed by an operator. During operation, the situation changes due to the movement of the robot: The hazardous area becomes the working area and vice versa.

The following monitoring cases are defined:

  • Case 1: While the robot works at station 1, 
the operator can load or unload at station 2.

  • Case 2: While the robot works at station 2, 
the operator can load or unload at station 1.

  



To monitor this assembly cell, a SICK safety laser scanner S3000 is to be used in conjunction with a fail-safe SIMATIC S7-1500 (F-CPU).

The laser scanner monitors a danger area, depending on the robot’s position, and shuts down its safe OSSD output (Output Signal Switching Device) upon entering the protective field, which causes the F-CPU to shut down the robot.



F-CPU and laser scanner communicate via PROFINET with the error-secure “PROFIsafe” profile. The robot’s position is detected via two sensors (e.g. SIRIUS position switch).

Downloads
  Documentation (1,0 MB) 
 Registrierung notwendig  Example project for TIA Portal V13 SP1, configuration file for SICK S3000 (12,8 MB) 


Archive
  Documentation V1.0 for S7-300 and TIA Portal V11 (1,4 MB)
 Registrierung notwendig  Example project V1.0 for S7-300 and TIA Portal V11 (2,3 MB)
 Registrierung notwendig  Configuration file V1.0 for SICK S3000 (7,5 KB)


Last Changes
Attachments of V1.0 of the application example re-added


Additional Keywords
Field set, warning field, protective field, Safety Advanced

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.