×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 58805543, Entry date: 03/13/2012
(0)
Rate

How can you replace the SINAMICS CU320 with the CU320-2 in a Technology CPU project with S7 Technology?

  • Entry
  • Associated product(s)

Description
As from version V4.2 SP1 of S7 Technology you have the option of automatically replacing the SINAMICS device version and characteristic in an existing S7 Technology project.

Instructions
Mark the required SINAMICS drive in the tree view and select the pop-up menu "Target device > Upgrade device version/characteristic".


Fig. 01

Then select the required characteristic from the list of available SINAMICS characteristics.


Fig. 02

Then select the required firmware version from the list of available device versions.


Fig. 03

Finally, click the "Upgrade" button to replace the SINAMICS control unit in the S7 Technology project with the version selected.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.