×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 58824610, Entry date: 07/06/2021
(1)
Rate

Integration SIMOCODE pro V with a Fail-safe Digital Module in SIMATIC PCS 7

  • Entry
  • Associated product(s)
This application example shows how a motor in connection with the process control system and a safety system is to be safely shut down safely in compliance with the requirements for SIL 2 and SIL 3 (SIL – Safety Integrity Level, standard: IEC 61508/IEC 62061).
Process industry often uses procedures that work with high pressures or temperatures.. The processed materials are often hazardous to people’s health or can destroy the environment when released.
In many cases a safety system is used if there is an intolerable risk for people or the environment. The safety system has the task to stop the process when a critical status is reached and to prevent an emission of hazardous materials. Blocking systems must be safely closed and supply units (pumps, ventilation systems, conveyor units) must be safely de-energized.

The flexible motor management system SIMOCODE pro V with the DM-F PROFIsafe module is used as a drive here. 

Benefits

The solution presented in this document provides you the following benefits:

  • Safety-oriented shut-down of a load by SIMOCODE pro V with DM-F PROFIsafe
  • uniting operational and fail-safe shut-down in the motor management system without any additional effort
  • broad scope of application with the safety integration level (IEC 61508) up to SIL 3
  • functions for a contactor monitoring in the SIMOCODE pro V modules
  • transmission of meaningful diagnose information to the AS and display in the OS
  • reduction of space needed for the installation in the control cabinet, since only a limited number of devices are used
  • standardized integration of the motor branch circuit and reduction of the wiring thanks to an integrated PROFIBUS DP interface

In the enclosed demo project you will find the following functions realized, wich you can use as template in your own projects for safing engineering time:

  • Hardware configuration with FH-CPU and SIMOCODE pro V DM-F PROFIsafe (PDM)
  • AS program with fail safe part and MOS function (Maintenance Override Switch) for testing and maintenance
  • OS project


Integration SIMOCODE pro V PN with a Fail-safe Digital Module in SIMATIC PCS 7 V9.0 SP3

The project was created with the following software components:

  • PCS 7 V9.0 SP3
  • S7 F Systems V6.3
  • SIMATIC PDM V6.0 SP5
  • SIMOCODE EDD for PDM
  • PCS 7 SIMOCODE pro library V9.0 SP3

  Documentation (3,9 MB)
 Registrierung notwendig  Demo Project (118,6 MB)(SHA-256)
The password for the fail-safe program is "Siemens!".


Further information

Motor Management and Control Devices SIMOCODE pro 3UF 
SIMATIC Prozessleitsystem PCS 7 Kompendium Teil B - Process Safety


Last Change

Update to PCS 7 V9.0 SP3


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.