×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 59600972, Entry date: 06/11/2012
(0)
Rate

When should you install the Hotfix 1 for the SIMATIC IPC DiagMonitor V4.3.3?

  • Entry
  • Associated product(s)

Description
If one of the following points applies for you, then you must install the SIMATIC IPC DiagMonitor V4.3.3 Hotfix 1.

  • Installation of the SIMATIC IPC DiagMonitor V4.3.3 on SIMATIC IPC547D
  • Call of diagnostics data with Microsoft Visual Studio and the DiagMonitor- API
  • Sporadic timeout when adding stations
  • Start phase takes too long for platforms that are not supported and are only for monitoring

Download
 

Drivers Download
HF1 DiagMonitor V4.3.3 DMHotfix_4331.zip ( 2506 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.