×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 60035096, Entry date: 09/25/2014
(1)
Rate

Creating Documentation Components for PROFINET IO Networks.

  • Entry
  • Associated product(s)
Problem For the system acceptance test you usually need a document which lists existing status of the PROFINET IO network at a fixed time and prints them in a suitable format. These are for example: project data, module status of all nodes, port status of all PROFINET IO devices, etc. This inform...
Problem
For the system acceptance test you usually need a document which lists existing status of the PROFINET IO network at a fixed time and prints them in a suitable format. These are for example: project data, module status of all nodes, port status of all PROFINET IO devices, etc. This information can be extracted and edited from the STEP 7 configuration files.

Solution  
With the help of the „Topology Reporter” tool you can create a document from the exported data of your STEP 7 project that displays all relevant data regarding the topology of your PROFINET IO network in a clear form. A typical field of application of this tool is e.g. the final documentation for the system acceptance test.

The following graphic shows you the data flow from plant network to the Topology Report.

The tool on hand offers you the following advantages:

  • creation of a complete documentation component of your PROFINET IO network
  • it is based on the consistent configuration file of the plant
  • This makes a new status comparison of the plant possible at any time
  • The tool can also used as Java application on non-Windows operating systems.

Attention
Use the Topology Reporter only with STEP 7 V5.5 up to and including SP3!

Downloads

Content of Downloads

Download

Documentation
Creating Documentation Components for PROFINET IO Networks.
60035096_Topology-Reporter_DOKU_V10_en.pdf ( 681 KB )
Code 
Tool Topology Reporter
60035096_Topology_Reporter_V10.zip ( 6041 KB )


To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Last Changes
First Edition


Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.