Delivery release for Drive ES Basic V5.5 SP1
-
Entry
-
Associated product(s)
With immediate effect, the product Drive ES Basic V5.5 SP1 has been released for delivery. This has been revised and enhanced due to the market launch of STEP7 V5.5 SP1 and SP2, the support for the operating system Windows 7 (64 bit) as well as an update of the integrated STARTER commissioning tool to Version V4.3 SP1.
Update dd Apr. 15, 2013
Delivery release has been granted on April 16, 2012
Ordering information for Drive ES Basic V5.5 SP1
Order number |
Designation |
6SW1700-5JA00-5AA0 |
Drive ES Basic V5.5 SP1 Single license |
6SW1700-5JA00-5AA1 | Drive ES Basic V5.5 SP1 Copy license (60 users at the same time) |
6SW1700-5JA00-5AA4 | Upgrade Drive ES Basic V5.x --> V5.5 SP1 Upgrade license |
6SW1700-0JA00-0AB2 | Software Update Service (SUS) for Drive ES Basic single license |
6SW1700-0JA00-1AB2 | Software Update Service (SUS) for Drive ES Basic copy license |
With immediate effect, the product Drive ES Basic V5.5 SP1 has been released for delivery. This has been revised and enhanced due to the market launch of STEP7 V5.5 SP1 and SP2, the support for the operating system Windows 7 (64 bit) as well as an update of the integrated STARTER commissioning tool to Version V4.3 SP1.
The following individual innovations have been made in the V5.5 SP1 compared to the previous version V5.5
- Support for the operating system Windows 7 (64 bit) in the Professional, Ultimate and Enterprise versions
- Fully compatible with STEP7 V5.5 SP1 and SP2
- The Starter Version V4.3 SP1, the commissioning tool for SINAMICS and 4th Generation MICROMASTER have been integrated.
- Communication to SINAMICS G120 drives with CU2xx-2 is also supported via USB (native)
- SimoCom A Version V 05.03.02, the tool for the POSMO A, has been integrated.
- SimoCom U Version 13.02.02.01, the tool for the SIMODRIVE 611U and POSMO CA/CD/SI, has been integrated.
- DriveMonitor Version V5.5, the tool for MASTERDRIVES and SIMOREG, has been integrated. (unchanged)
Benefits provided by a Drive ES Basic installation compared to the installation of individual tools
- Benefits provided compared to all single tools (STARTER Stand alone, SIMOCOM U/A and DriveMonitor)
- More convenient integration of the drives in the hardware configuration of SIMATIC S7 via object manager (SlaveOM and DeviceOM) instead of GSD files
- The communication can also be set up beyond network boundaries by routing in the SIMATIC and SIMOTION stations. Without Drive ES, the individual tools can only communicate with drives that are connected to the same subnet (PROFIBUS, PROFINET) as the engineering PC/PG. Please read the routing notes!
- The tools can be directly called up in a context-sensitive manner from the SIMATIC Manager. All the necessary network information is automatically transferred for routing.
- Further advantages compared to DriveMonitor and SIMOCOM U/A
- Data archiving in the S7 project
- Another advantage compared to DriveMonitor
- Direct communication via PROFIBUS
Without Drive ES, the DriveMonitor can only communicate with the drives via USS protocol via a serial interface or via a PROFIBUS-OPC server
- Direct communication via PROFIBUS
Routing notes
Routing-capable modules support routing to the drives beyond network boundaries.
- Routing in combination with SIMOTION:
All SIMOTION modules support the functionality "Routing/S7-Routing", but not the functionality "Data record routing".
Thus, new G120 devices cannot be reached via routing with a CU2xx-2 behind a SIMOTION. - Routing in combination with SIMATIC S7:
The "S7 routing-capable" SIMATIC modules are listed under 584459 or directly in the hardware catalog of the STEP7 hardware configuration.
For routing to the new G120 devices with CU2xx-2, you require SIMATIC modules which, additionally to S7-Routing, also support the functionality "Data record routing".
General information regarding data record routing is provided under 7000978. SIMATIC modules which support data record routing are listed under 50037141.
![]()
Fig. 01: Information screen with routing data
Innovations regarding the integrated Starter V4.3 SP1
The newly integrated Starter V4.3 SP1 ( V4.3.1.0 ) supports the following drive systems:
- 4th Generation MICROMASTER
- SINAMICS DCM with Firmware V1.1 and V1.2 and V1.3
- SIMATIC ET200S FC with Firmware V1.0.x and V3.0.x
- SIMATIC ET200pro FC with Firmware V3.0.x
- SINAMICS G110 with Firmware V1.0.x and V1.1.x
- SINAMICS G110D with Firmware V3.3.x and V3.4.x
- SINAMICS G120 with Firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x, V4.2, V4.3.0, V4.3.2 and (with SSP) V4.5
- SINAMICS G120C with Firmware (with SSP) V4.5
- SINAMICS G120D with Firmware V3.0.x, V3.1.x, V3.2.x and (with SSP) V4.5
- SINAMICS G120P with Firmware V4.2, V4.3.0, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G120P BT with Firmware (with SSP) V4.4.1
- SINAMICS G130 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G130 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.5
- SINAMICS G150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G150 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.5
- SINAMICS GM150 with Firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GM150 with Firmware V4.3.1 and (with SSP) V4.5
- SINAMICS GL150 with Firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GL150 with Firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS S110 with Firmware V4.1, V4.3.1, V4.3.2 and (mit SSP) V4.4
- SINAMICS S120 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S120 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS S150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S150 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS SL150 with Firmware V4.3.1, V4.4.2 and (with SSP) V4.4
- SINAMICS SM120 with Firmware (with SSP) V4.4.2
- SINAMICS MV with Firmware (with SSP) V4.5
Further information regarding the integrated Starter Version V4.3 SP1 is provided under 59441514.
The integrated commissioning tools can also be downloaded individually from the Internet and can be used as a free upgrade for an existing Drive ES Basic V5.4 SPx installation.
How to obtain the new Drive ES Basic Version?
- New order!
- With this delivery release, all orders placed for the Version V5.5 SP1 will be delivered. The price remains unchanged compared to the previous versions.
- For users who have already purchased a Drive ES Basic V5.x version!
- They can order the upgrade version which is offered at a significantly lower price than the full version. Due to limited memory space, you cannot download the complete Drive ES Basic DVD V5.5 SP1.
- For users who have subscribed to the Software Update Service 6SW1700-0JA00-0AB2 resp. 6SW1700-0JA00-1AB2!
- Users who have already subscribed to the Software Update Service will automatically receive the new version. More detailed information regarding Software Update Service processing is provided under 13532008.
Operating systems and STEP7 compatibility
Drive ES Basic can be used with the following Microsoft operating systems:
- Microsoft Internet Explorer V6.0 (or later)
- 32-bit operating systems
- Microsoft Windows Server 2003 SP2
- Microsoft Windows Server 2008
- Microsoft Windows XP Professional SP2 *) and SP3
- Microsoft Windows 7 Professional incl. SP1
- Microsoft Windows 7 Ultimate incl. SP1
- Microsoft Windows 7 Enterprise incl. SP1 (Standard Installation)
- 64-bit operating systems***)
- Microsoft Windows 7 Professional SP1
- Microsoft Windows 7 Ultimate SP1
- Microsoft Windows 7 Enterprise SP1 (Standard Installation)
- Microsoft Windows Server 2008 R2 SP1**)
*) limited test scope
**) Additional compatibily test took place; Installation is possible after confirming the warning message.
***) IMPORTANT
With 64-bit operating systems, the special driver for the transition/special protocol "USS via USB" is available after installing HotFix 5 (see 26233208). However, this only concerns a few SINAMICS G120 with CU2xx-2 and Firmware Version V4.2 or V4.3..
Drive ES Basic can be used with the following STEP7 versions:
- STEP7 V5.3 SP1 (or later)
- STEP7 V5.4 SPx
- STEP7 V5.5 SPx.
More detailed information regarding the compatibility is included under 18495518.
Languages supported:
- German
- English
- French
- Italian
- Spanish
Note
In Version V5.5 (or later), Drive ES Basic is only provided as a mere option package for SIMATIC STEP7, that means the Drive ES Basic V5.5 (or later) can only be installed additionally to an already installed STEP7 full version. The procedure remains the same for SIMATIC-S7 users.
The Version V5.5 can, however, no longer be used with a STEP7 independent stand-alone installation. The stand-alone installation is no longer supported as from the Drive ES Basic Version V5.5.
Product cancellation for the product Drive ES Basic V5.3
Upon release of the new Version V5.5 SP1, all previous versions are discontinued and phased out.
This means that the ordered units affected are no longer listed in the catalog, but will still be delivered as a spare part for approx. one year:
Order number | Designation |
6SW1700-5JA00-3AA0 | Drive ES Basic V5.3 SPx Single license |
The following order numbers are discontinued:
Order number | Designation |
6SW1700-5JA00-3AA1 | Drive ES Basic V5.3 SPx Copy license (60 users at the same time) |
6SW1700-5JA00-3AA4 | Upgrade Drive ES Basic V5.x --> V5.3 SPx Upgrade license |
For more detailed information, please contact your local Siemens office.
- German
- Chinese
Entry belongs to product tree folder(s):
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry