×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 60162195, Entry date: 06/02/2015
(20)
Rate

TIA Portal Readiness Check Tool

  • Entry
  • Associated product(s)
The TIA Portal Readiness Check Tool offers an easy way to check if the hardware included in projects is supported by TIA Portal. The tool can be used for: STEP 7 V5.4 STEP 7 V5.5 WinCC V7 WinCC flexible 2008 ...


Description

The TIA Portal Readiness Check Tool offers an easy way to check if the hardware included in projects is supported by TIA Portal. The tool can be used for:

  • STEP 7 V5.4
  • STEP 7 V5.5
  • WinCC V7
  • WinCC flexible 2008

Procedure

To use the TIA Portal Readiness Check Tool, unzip it and start the file "Readiness Check Totally Integrated Automation Portal.exe":

  • Once the tool has started, you can select the user interface language.
  • You can enter the module data in different ways:
    • As .cfg file
    • List with order numbers as .xls
    • List with order numbers as .csv
    • Manually enter order numbers
  • The modules supported by TIA Portal and those that are not supported are then displayed as result; for the latter you will see successor modules.
  • There is also a list of the engineering software products that can be used to edit the hardware components.

Notes on included Open Source software components

The TIA Portal V13 SP1 Readiness Check Tool also includes Open Source software components.

See the Readme OSS for more information.
   readme_oss.pdf (261,6 KB)

The software of an included Open Source component is available here:
OpenSourceSoftware.zip (2607 KB)

Download TIA Portal Readiness Check Tool V1.21

This free download includes the TIA Portal V13SP1 Readiness Check Tool for checking the hardware support of the TIA Portal V13 SP1.

*** New *** in TIA Portal Readiness Check Tool V1.21:
-Display of supported hardware for SIMOTION SCOUT TIA V4.4

Readiness_Check_Totally_Integrated_Automation_Portal_V1_21.zip (2.6 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.