×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 60546560, Entry date: 03/06/2018
(1)
Rate

PCS 7 Unit Template "Stirred Tank Reactor" using the example of the Chemical Industry

  • Entry
  • Associated product(s)
The unit template "Stirred Tank Reactor" is based on a standardized and structured design of the automation program through the use of predefined equipment and control modules. The example is used both as a basis for projects and as an overall standardization template.

The standardization of automation engineering for processing plants, such as in the chemical industry, is a major challenge. Different process steps and procedures, different equipment and flexibility in the production make the task even more difficult. This includes the plant structure according to the ISA-106. This specifies the lower four levels, i.e. plant area, unit, equipment and device. A plant area always consists of units. The units contain standardized equipment modules.

The unit template provides a template that comprises all typical components of a stirred tank reactor, their open- and closed-loop control, the necessary logic and interlocking as well as the visualization. It is modularly structured and based on standardized equipment modules.

Its use offers the following advantages:

  • A reduction in the expertise necessary to develop applications

  • A decrease in the configuration effort

  • More flexible setup and adaptation due to equipment modules

  • Standardized structures



A stirred tank reactor as part of a process plant

Validity
SIMATIC PCS 7 V9.0 and PCS 7 V8.0

Documentation and Sample Project for PCS 7 V9.0
  Documentation (3,5 MB)

You can download the example project for PCS 7 V9.0 in the Extranet-section of this entry. This Extranet section is only visible if have concluded a Managed System Services contract. Refer to the following link for detailed information: Managed System Services.

Documentation and Sample Project for PCS 7 V8.0
  Documentation (3,9 MB)
 Registrierung notwendig  PCS 7 V8.0 sample project (77,1 MB)

Further Information
Equipment Modules for PCS 7 using the example of the Chemical Industry
Simulation of a PCS 7 stirred tank reactor with SIMIT Simulation Framework
PCS 7 Unit Template "Distillation Column" using the example of the Chemical Industry
PCS 7 Unit Template "Polymerization Reactor" using the example of the Chemical Industry
PCS 7 Unit Template "Dryer" using the example of the Chemical Industry
PCS 7 Unit Template "Fermenter" using the example of the Chemical Industry
Integration of Advanced Process Graphics in SIMATIC PCS 7
Service Contracts - SIMATIC PCS 7 Lifecycle Services
Managed System Services overview page

Last revision
Update to PCS 7 V9.0, Integration of Smart Alarm Hiding, Managed System Services Extranet section

Additional keywords
Technical function, function, modules, control module, function group, process tags, process tag types

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.