×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 61003253, Entry date: 10/17/2012
(0)
Rate

Delivery release for SIMOTION Version V4.3 SP1 HF3 and SIMOTION D410-2 DP/PN

  • Entry
  • Associated product(s)

With immediate effect, the SIMOTION Version V4.3 SP1 HF3 incl. SIMOTION D410-2 DP/PN has been released for delivery.

This release includes the Engineering System SIMOTION SCOUT and SCOUT Stand-alone V4.3 SP1 HF3 as well as the SIMOTION Runtime Software V4.3 SP1 HF3, which is supplied with the SIMOTION SCOUT.

Contents

1. General information

2. Scope of functions

3. Compatibility

4. Test certificates

5. Components released

6. SIMOTION SCOUT / SIMOTION Software Update Contracts delivered

1. General information

SIMOTION V4.3 SP1 HF3 incl. SIMOTION D410-2 DP/PN have been released for delivery with immediate effect. We generally recommend that you use the Version V4.3 SP1 HF3.

The release refers to the following components:

  • Engineering System SIMOTION SCOUT and SCOUT Stand-alone V4.3 SP1 HF3
  • SIMOTION Kernel/Firmware V4.3 SP1 HF3 (supplied with SIMOTION SCOUT)
  • SIMOTION D410-2 DP/PN

Users who have already concluded a valid Software Update Service contract for SCOUT and SCOUT Stand-alone automatically receive SIMOTION SCOUT/SCOUT Stand-alone V4.3 SP1 HF3 (on DVD).
All licenses for SCOUT V4.3 remain valid.

With immediate effect, the Control Units SIMOTION D4xx and D4xx-2 with Software Version V4.3 SP1 HF3 have been released. The CF cards for SIMOTION D4xx (6AU1400-2PA02-0AA0), SIMOTION D410-2 (6AU1400-1PA22-0AA0) and SIMOTION D4x5-2 (6AU1400-2PA22-0AA0) will be supplied with the SIMOTION Kernel V4.3 SP1 HF3.

With immediate effect, SIMOTION C240/C240 PN with Software Version V4.3 SP1 HF3 has been released. The MMC card for SIMOTION C240/C240 PN (6AU1720-1KA00-0AA0) will be supplied with the SIMOTION Kernel V4.3 SP1 HF3.

With immediate effect, SIMOTION P320-3 and SIMOTION P350-3 with Software Version V4.3 SP1 HF3 have been released.
SIMOTION P320-3 will continue to be released ex factory with the SIMOTION Kernel V4.3 SP1 HF1. The Kernel V4.3 SP1 HF3 will be supplied on the SCOUT DVD and can be used to upgrade the SIMOTION P320-3 to the Version V4.3 SP1 HF3.
SIMOTION P350-3 will be released ex factory with the SIMOTION Kernel V4.3 SP1 HF3. The Kernel V4.3 SP1 HF3 will be supplied on the SCOUT DVD and can be used to upgrade the SIMOTION P350-3 to the Version V4.3 SP1 HF3.

2. Scope of functions

Various functional restrictions (details see SCOUT Readme file) in the Engineering System and in the Runtime Kernels have been corrected in SIMOTION V4.3 SP1 HF3.

Further, the Version V4.3 SP1 HF3 is required to use the component

  • SIMOTION D410-2 DP/PN, see also 60997586

As from SIMOTION V4.3 SP1 HF3, the PROFIsafe Telegrams 31 and 901 have also been released, in addition to Telegram 30, for SIMOTION D410-2. Information regarding the new functions included in Version V4.3 SP1 is provided in 61002935.

The STARTER Version V4.3 SP1 HF2 is integrated in the Engineering System SIMOTION SCOUT and SCOUT Stand-alone V4.3 SP1 HF3 (see also 61585426).

The setup of the SIMOTION SCOUT and SCOUT Stand-alone V4.3 SP1 HF3 is a complete setup (not a delta setup), that means the installation duration corresponds to the duration of a new installation.

3. Compatibility

The SIMOTION SCOUT Version V4.3 SP1 HF3 is compatible with the Versions V4.2, V4.1, V4.0 and V3.2.

Projects which have been created with older versions

  • can be upgraded to the new version (e.g. if the existing project shall be extended by the functions included in the Version V4.3 SP1 HF3). The relevant description is included in the Readme resp. in the manual.
  • can also be processed with the SCOUT Version V4.3 SP1 HF3 (only the project data are converted upwards, the Runtime remains unchanged). If required, you can then store again the project data in the formats V4.2, V4.1, V4.0 and V3.2. Projects being created under V3.0 or V3.1 must first be upgraded to the Version V3.2 (or later) using an older SCOUT version.

The current SIMOTION compatibility list including the combined software and hardware is provided in 18857317.

Remark regarding the TopLoading Application

The Toploading Application V1.9 is required when using the TopLoading Application with SIMOTION V4.3 SP1 HF3. As from SIMOTION V4.2 SP1, the Application Version V1.8 is no longer supported due to various interface changes.

4. Test certificates

The SINAMICS Safety Integrated functions provided by SINAMICS/SIMOTION are usually certified by independent institutes. You can obtain a list of the currently certified components from your local Siemens office. If you have any questions regarding certifications which have not yet been completed, please contact your local Siemens representative.

The SIMOTION D CompactFlash Cards are supplied with the Kernel/Firmware V4.3 SP1 HF3 and SINAMICS Integrated drive software.

SIMOTION D Kernel/Firmware Versions V4.3 SP1 HF3

SINAMICS Integrated drive software version V2.6 SP2 HF17
(V02.60.45.27)
V4.5 HF6
(V04.50.30.09)
Firmware Version "Safety Integrated Basic Functions" V02.60.40.00 (CU) V04.50.30.05 (CU)
Firmware Version "Safety Integrated Extended Functions" V02.60.45.13 (CU) V04.50.30.05 (CU)
Control Units supported D410, D425, D435, D445-1, CX32 D410-2, D425-2, D435-2, D445-2, D455-2, CX32-2

The current status of available certificates regarding international standards as well as machine safety (German Technical Inspectorate (TÜV), German Institute for Occupational Health and Safety (BGIA)) is provided at the following lnk: http://support.automation.siemens.com/WW/view/de/13305690/134200.

5. Components released

SIMOTION SCOUT

Order numbers Designation Version
6AU1810-1BA43-1XT7 SIMOTION Engineering System SCOUT V4.3 SP1 HF3 DVD, Demo/Trial Version with Trial License V4.3 SP1 HF3
6AU1810-1CA43-1XT7 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF3 DVD, Demo/Trial Version with Trial License V4.3 SP1 HF3
6AU1810-1BA43-1XA0 SIMOTION Engineering System SCOUT V4.3 SP1 HF3 DVD, with full license (Floating License) V4.3 SP1 HF3
6AU1810-1BA43-1XE0 SIMOTION Engineering System SCOUT V4.3 SP1 HF3 Upgrade DVD, with Upgrade License V4.3 SP1 HF3
6AU1810-1CA43-1XA0 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF3 DVD, with full license (Floating License) V4.3 SP1 HF3
6AU1810-1CA43-1XE0 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF3 Upgrade DVD, with Upgrade License V4.3 SP1 HF3

SIMOTION D

Order numbers Designation Version/Remark
6AU1400-2PA02-0AA0 1 Gbyte CompactFlash Card (CF) for SIMOTION D4xx
incl. SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be pre-licensed via Z options

Remark: Only for SIMOTION D4xx

V4.3 SP1 HF3

(SINAMICS V2.6 SP2 HF17)

6AU1400-2PA22-0AA0 1 Gbyte CompactFlash Card (CF) for SIMOTION D4x5-2
incl. SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be pre-licensed via Z options

Remark: Only for SIMOTION D4x5-2

V4.3 SP1 HF3

(SINAMICS V4.5 HF6)

6AU1400-1PA22-0AA0 1 Gbyte CompactFlash Card (CF) for SIMOTION D410-2
incl. SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be pre-licensed via Z options

Remark: Only for SIMOTION D410-2

V4.3 SP1 HF3

(SINAMICS V4.5 HF6)

Remarks The Firmware V4.3 SP1 HF3 is supplied with the SIMOTION SCOUT. Further, the firmware can be downloaded from the Product Support, see 31045047.

Further details regarding the Control Units D410-2, D425-2 and D435-2 are provided in 60997586.

The SIMOTION D445, order no. "6AU1445-0AA00-0AA0", is no longer supported as from Runtime System V4.3. With SCOUT V4.3, however, the Control Unit can be configured with a Runtime System < V4.3.

SIMOTION C

Order numbers Designation Version/Remark
6AU1720-1KA00-0AA0 MMC 64MB for SIMOTION C240 / C240 PN with SIMOTION Kernel/Firmware; can be pre-licensed via Z options V4.3 SP1 HF3
Remarks The Firmware V4.3 SP1 HF3 is supplied with the SIMOTION SCOUT. Further, the firmware can be downloaded from the Product Support, see 31263919.

The C230-2, order no. "6AU1230-2AA01-0AA0" is no longer supported as from Runtime System V4.2. With SCOUT V4.3, however, it can be configured with a Runtime System < V4.2.

SIMOTION P

Order numbers Designation Version/Remark
6AU1350-3AK41-1BE2 - Z V43 W01 SIMOTION P350-3 PROFIBUS, Pentium M 2GHz, without DVD-ROM

SIMOTION P350-3 is supplied ex factory with SIMOTION Kernel V4.3 SP1 HF3. The Kernel V4.3 SP1 HF3 is provided on the SCOUT DVD and can be used to upgrade the SIMOTION P350-3 to the Version V4.3 SP1 HF3.

 

SIMOTION P320-3 are continued to be supplied ex factory with SIMOTION Kernel V4.3 SP1 HF1. The Kernel V4.3 SP1 HF3 is provided on the SCOUT DVD and can be used to upgrade the SIMOTION P320-3 to the Version V4.3 SP1 HF3.

6AU1350-3AK43-1BE2 - Z V43 W01 SIMOTION P350-3 PROFIBUS, Pentium M 2GHz, with DVD-ROM
6AU1350-3AK41-2BE2 - Z V43 W01 SIMOTION P350-3 PROFINET, Pentium M 2GHz, without DVD-ROM
6AU1350-3AK43-2BE2 - Z V43 W01 SIMOTION P350-3 PROFINET, Pentium M 2GHz, with DVD-ROM
6AU1320-7AB55-3AF0 SIMOTION P320-3 PROFINET, INTEL CORE 2 SOLO 1.2 GHZ WITH WINDOWS EMBEDDED STANDARD 2009

Device Update Tool/Firmware Support Package

With the Device Update Tool for upgrading  SIMOTION devices, SIMOTION provides a user-friendly solution. The Firmware Support Package V4.3 SP1 HF3 is supplied with the SIMOTION SCOUT. Further, the Firmware Support Package for SIMOTION D and SIMOTION C can be downloaded from the Product Support, see 33119786.

6. SIMOTION SCOUT / SIMOTION SCOUT Software Update Contracts delivered

SIMOTION SCOUT

The SIMOTION SCOUT Version V4.3 SP1 HF3 requires the Version STEP7 V5.5 SP2 as option package for STEP7. SCOUT Stand-alone V4.3 SP1 includes the STEP7 components of the Version V5.5 SP2. SCOUT and SCOUT Stand-alone have been released for the operating systems Windows XP SP3, Windows 7 Professional and Ultimate (32-bit and 64-bit).

The SIMOTION SCOUT software versions must be ordered stating the above-listed order numbers. Orders placed for new parts stating older versions are automatically substituted by SIMOTION Version V4.3 SP1. If older SCOUT versions are requested, these must be ordered as spare part.

SIMOTION SCOUT Software Update Contracts

Users who have already signed a valid Software Update Service contract for SCOUT or SCOUT Stand-alone automatically receive SCOUT or SCOUT Stand-alone V4.3 SP1 HF3 (on DVD). Users who have not concluded a Software Update Service contract can order the current software version stating the above-mentioned order numbers.

For more detailed information, please contact your local Siemens office.

SIMOTION CamTool

The Software CamTool V3.0 SP2 is included in the complete SCOUT or SCOUT Stand-alone package, the necessary license must be ordered separately. All existing CamTool V3.0 licenses remain, of course, valid. Licenses for CamTool lower V3.0 must be upgraded to the current Version 3.0 by ordering an upgrade (6AU1810-0FA30-2XE0).

SIMOTION DCC

The relevant product DCC SIMOTION with license must be ordered before it can be used. DCC SIMOTION comprises the license for DCC SIMOTION and DCC SINAMICS. Licenses for V2.1 which have already been delivered remain valid for V2.2 SP1. Already delivered licenses for V2.0 require an upgrade license. With the setup for SCOUT V4.3 SP1, the DCC libraries (DCB) are automatically installed and optionally also the DCC Editor (CFC V8.0). The orderable DCC DVD need not be installed separately.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.