×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 61450284, Entry date: 06/24/2019
(15)
Rate

24V load circuit monitoring with SITOP PSE200U single-channel signaling and SIMATIC S7 CPUs

  • Entry
  • Associated product(s)
The SITOP PSE200U selectivity module with single-channel signaling enables you to monitor 24V load circuits.

The signal at the state output (S) of the SITOP PSE200U module provides serially encoded information on the state of the load circuits connected to the outputs OUT 1 thru OUT 4 of the SITOP PSE200U module. A SIMATIC S7 CPU shall be used to acquire and monitor the status of the load circuits.

Solution
The present document includes a collection of block libraries and library descriptions for SIMATIC S7-300/S7-400 and SIMATIC S7-1200/S7-1500. The library blocks are used to read and evaluated the signal of the state output (S) via a digital input at the S7 CPU. You may display this information e.g. as a message on an operator panel, as a potential application. The needed digital inputs and outputs can be located in a Distributed I/O (e. g. ET 200SP).

Note
The library blocks for S7-300/S7-400 can be used in an ET 200S IM 151-8(F) PN/DP CPU and ET 200pro IM 154-8(F/FX) PN/DP CPU. The library blocks for S7-1200/S7-1500 can be used in an ET 200SP CPU.

The figure below shows the solution in the form of a graph.
 

   
Library
  Documentation LSitop Library STEP 7 V5 (1,3 MB)
  Documentation LSitop Library STEP 7 V14 and higher version (1,4 MB)
 Registrierung notwendig  Library for STEP 7 V5 (34,1 KB)
 Registrierung notwendig  Library for STEP 7 V15 (855,1 KB)
 Registrierung notwendig  Library for STEP 7 V14 (2,8 MB)
 Registrierung notwendig  Library for STEP 7 V13 SP1 (1,3 MB)

Last changes

  • Complete revision of the library blocks and the documentation
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.