×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 61450284, 文档发布日期 2018年6月26日
(15)
评估

24V load circuit monitoring with SITOP PSE200U single-channel signaling and SIMATIC S7 CPUs

  • 文档
  • 涉及产品
The SITOP PSE200U selectivity module with single-channel signaling enables you to monitor 24V load circuits.

The signal at the state output (S) of the SITOP PSE200U module provides serially encoded information on the state of the load circuits connected to the outputs OUT 1 thru OUT 4 of the SITOP PSE200U module. A SIMATIC S7 CPU shall be used to acquire and monitor the status of the load circuits.

Solution
The present document includes a collection of block libraries and library descriptions for SIMATIC S7-300/S7-400 and SIMATIC S7-1200/S7-1500. The library blocks are used to read and evaluated the signal of the state output (S) via a digital input at the S7 CPU. You may display this information e.g. as a message on an operator panel, as a potential application. The needed digital inputs and outputs can be located in a Distributed I/O (e. g. ET 200SP).

Note
The library blocks for S7-300/S7-400 can be used in an ET 200S IM 151-8(F) PN/DP CPU and ET 200pro IM 154-8(F/FX) PN/DP CPU. The library blocks for S7-1200/S7-1500 can be used in an ET 200SP CPU.

The figure below shows the solution in the form of a graph.
 

   
Library
  Documentation LSitop Library STEP 7 V5 (1,3 MB)
  Documentation LSitop Library STEP 7 V14 (1,4 MB)
 Registrierung notwendig  Library for STEP 7 V5 (34,1 KB)
 Registrierung notwendig  Library for STEP 7 V14 (7,2 MB)
 Registrierung notwendig  Library for STEP 7 V13 SP1 (1,3 MB)

Last revision

  • Complete revision of the library blocks and the documentation
安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.