×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 61705616, Entry date: 06/25/2012
(0)
Rate

What is required to run SITRANS DTM?

  • Entry
  • Associated product(s)

Question:
What is required to run SITRANS DTM?

Answer:
Before installing SITRANS DTM, you must have already installed a Field Device Tool (FDT) such as PACTware or Fieldcare. Then you can install SITRANS DTM which can be downloaded from www.siemens.com/sitransdtm and then choose Support, and then Software downloads. After installing SITRANS DTM, you then need to install the EDDs for SITRANS DTM for the instruments that you want to use DTM to communicate with.  Please note that you will also need some sort of communication DTM such as a HART modem DTM or a PROFIBUS communication DTM depending on your communication method. 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit