×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 61909867, Entry date: 07/11/2012
(0)
Rate

Hotfix 02.04.01.01 for the MCIS DNC SW Version 02.04.01, June 2012

  • Entry
  • Associated product(s)

The Hotfix 02.04.01.01 is an update for the MCIS-DNC Software Version 02.04.01

Changes compared to SW 02.04.01.01

The following errors have been corrected:

  • DNC_IFC keyswitch function not operational in the current DNC operation
  • DNC IFC setup on MMC 103

Note

  • The Repair function can still be accessed by clicking on the Support Information under Add or Remove Programs

  • If the DNC IFC is installed on a new Windows (that means, not updated), the setup is terminated and an incorrect error message output

  • If the DNC IFC is installed on an existing DNC IFC 2.4.1.0, some data are reinstalled when starting the DNC IFC via Programs -->MCIS DNC

Installation requirements

This software may only be installed on MCIS DNC SW 02.04.01.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.