×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 61926069, Entry date: 08/02/2012
(1)
Rate

Fluidized Bed Dryer - Design of Model Predictive Control with Economical Steady State Optimization

  • Entry
  • Associated product(s)

Objective of the Application
The functionality of the model predictive controller provided in SIMATIC PCS 7 (function blocks ModPreCon and MPC) is extended with PCS 7 V8.0. Its new features are introduced in this application note.

This application note is an extension of the application note "Multivariable Model Predictive Control – the Distillation Column as an Application Example" (ID: 37361208), containing basic information how to apply the MPC.

The application example considered here shows an MPC with two manipulated -, two controlled - and three measurable disturbance variables in combination with a simulated process of a fluidized bed dryer.

Main Contents of this Application Note
The following issues are discussed in this application note:

  • Automatic process excitation to generate identification data, using the new function block "AutoExcitation"
  • Using prior knowledge for model generation in new MPC configurator
  • Robust controller design considering model quality
  • Generation of reports on controller design
  • Application of steady state working point optimization integrated in "ModPreCon"-function block to minimize energy consumption while keeping product quality within constraints
  • Simulation example fluidized bed dryer

Validity
… valid from PCS 7 V8.0

Downloads

Contents of the downloads

Download

Documentation 
Fluidized Bed Dryer - Design of Model Predictive Control with Economical Steady State Optimization
61926069_MPC_Robust_en.pdf ( 1698 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit