×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 62102847, Entry date: 12/12/2013
(0)
Rate

EDD: SITRANS LUT400 - HART - SITRANS DTM

  • Entry
  • Associated product(s)
Engineering Tool: SITRANS DTM
Tool Version: ≥ 3.1
Supported Firmware: ≥ 1.00.00
EDD Version: 1.00.00
Order number: 7ML5050-0****-***0
Hardware Version: 1.00.00
Firmware Version: 1.00.00

SITRANS DTM - powered by EDDL
 
 
This installation file requires the software SITRANS DTM. SITRANS DTM has to be installed only once and can be downloaded from product support under the following link:
http://support.automation.siemens.com/WW/view/en/53754140
 
After the installation of SITRANS DTM any desired device EDD can be installed.
To install the device EDD unzip it, then double-click on the .exe file and follow the instructions.
More information about the installation can be found under the following link:
http://support.automation.siemens.com/WW/view/en/61705616
 
More information about SIEMENS process instrumentation:
www.siemens.com/fielddevices
 


By downloading this file you accept the underlying Terms of Use.

  SITRANS_LUT400_HA_DTM_FDT_1_00_00_06.zip ( 1069 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit