×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 62561371, Entry date: 10/10/2018
(10)
Rate

IdentSNAPSHOT Version 2.0 HF1

  • Entry
  • Associated product(s)
Software for the registration of machines and plants with products of different product families, e.g. SINUMERIK, SIMOTION, SINAMICS und SIMATIC.

Description
We place a lot of emphasis on the satisfaction of our customers and optimum service. This starts with the consultation before the actual purchase of a machine equipped with control and drive technology from Siemens up to service after purchase. However, in most cases as system supplier, we do not know the final destination of the plants, machines or systems – equipped with Siemens technology – after the manufacturer has shipped them to the operating company. However, also for these machines, we want to further improve the service and support that we offer.

Everything that you have to do to achieve this: Register your machine online with us.

You benefit from:

  • even better services for registered machines
  • faster response times when service is required for machines that have been registered
  • higher productivity in your production

Prolongation of the on-site service for SINUMERIK 828D or 808D
For machines equipped with a SINUMERIK 828D or 808D control system, by registering your machine, you can simply extend the free-of-charge on-site service from 24 months up to 36 months. The on-site service includes the material and the service itself. A detailed description is provided at the following link: www.siemens.com/automation/oss

To register your plants or machines, all you require is the software

 Registrierung notwendig  identSNAPSHOT_V02.00.00.01_x86.zip (67,8 MB)

a function to facilitate direct and secure data transfer! After it has been uploaded, the new version of identSNAPSHOT provides you with a registration certificate (along with the confirmation of receipt), so that you obtain a precise list of all of the registered articles with the associated serial numbers for your documentation.


 

Preconditions

Hardware
IdentSNAPSHOT can run on any standard PC, PG or laptop that is capable of accessing the Internet.

Software
IdentSNAPSHOT is released for:

  • Windows XP SP3
  • Windows 7
  • Windows 8
  • Windows 10

.NET Framework V4.6 or higher must be installed on the PC.

Installation
identSNAPSHOT can be directly used by simply downloading a zip file – then you only have to register once and data can already be transferred.

Dokumentation
  identsnapshot_user_manual_en.pdf (1,0 MB) 

ReleaseNotes
 Registrierung notwendig  Release_Notes.txt (6,0 KB)

SW-Download
 Registrierung notwendig  identSNAPSHOT_V02.00.00.01_x86.zip (67,8 MB)
SHA-256 checksum:  Registrierung notwendig  identSNAPSHOT_V02.00.00.01_x86_Checksum.txt (1 KB)

Web Based Trainings
 Registrierung notwendig  62561371_web_based_trainings.zip (18,6 MB)

Note
Machine manufacturers can request predefined address information from their regional sales partners, including for their end customers, for importing into the software. This greatly facilitates the handling of address information when creating the final destination certificate and at the same time ensures a high level of data quality.
Contacts worldwide

Support
If you have any questions or problems when using IdentSNAPSHOT, then please contact
esupport.motioncontrol@siemens.com

Last change
10/2018

Supplementary search terms
EUNA, GSP, XML upload, XML

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit