×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 62883732, Entry date: 03/21/2014
(0)
Rate

SINAMICS G: Line Contactor Control using the ON/OFF1 Command for G120

  • Entry
  • Associated product(s)

Task
SINAMICS G120 converters are designed to be directly connected to the line supply; neither a line nor input contactor is required. However, for some applications a line contactor may be necessary. 

Solution
A circuit is described, which allows the line contactor to be automatically opened and closed via a digital output contact in the converter Control Unit. The line contactor is switched using the ON/OFF1 command of the converter. This ON/OFF1 command can be received from every active converter command source. Optionally, the line contactor can be opened each time that the converter is switched-off, for example, as a result of a fault. No external components are required to implement the control. However, the permissible switching power (switching rating) of the digital output contact and the closing/holding power of the line contactor solenoid must be checked. It may be necessary to use an auxiliary contactor/relay.

Delimitation
This document does not include any specifications regarding how the

  • the converter is configured
  • the basic commissioning of the converter
  • higher-level controls for commissioning

It is assumed that readers have a basic knowledge of these topics.

This solution can be used for:

  • SINAMICS G120 with Control Units CU230P-2, CU240x-2, CU250S-2 and firmware from version 4.4
    (An external 24 V power supply must be connected to the converter via terminals 31 and 32 of the Control Unit)

This solution cannot be used for:

  • SINAMICS G120C with firmware release v4.4
  • SINAMICS G120 up to and including firmware release v3.x

For these drives, parameter p0857 cannot be accessed, with which the monitoring time for the DC link pre-charging can be set (i.e. extended).
As a result of the excessively low DC link voltage, the converter quickly goes into the "Fault" state when the ON/OFF1 command is issued.

Downloads

Content of Downloads

Download

Documentation
Line Contactor Control using the ON/OFF1 Command for
SINAMICS G120
62883732_MainContactorControl_v1_1_en.pdf ( 159 KB )

Further Information
For MICROMASTER 4 and SINAMICS G120 with Firmware (FW) V3.x please use the following link.

Title

Entry-ID:

MICROMASTER, SINAMICS G: Controlling main contactor by using free function blocks (FFB) 22078212

Last Changes
Editorial revision

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.