×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 62883794, Entry date: 11/26/2012
(0)
Rate

Service Pack 2 incl. Update 1 for SIMATIC CFC V8.0 Released for Delivery

  • Entry
  • Associated product(s)

Service Pack 2 (SP2) incl. Update 1 is now available for SIMATIC CFC V8.0, which is embedded in the standard engineering software of the SIMATIC PCS 7 V8.0 process control system. The update is only available for download (see Download entry ID 62883989). It is of no relevance to the SIMATIC CFC V8.0 employed in the TIA environment.

With the Service Pack 2 incl. Update 1 the technological editor of SIMATIC CFC V8.0 will additionally support:

  • Integrated Engineering with COMOS V10.0
    • Transfer of instance-specific interlock circuits
    • Bi-directional exchange of SIMATIC PCS 7 messages
  • Individual control units and individual control types that contain hierarchical charts
  • Matching of individual control units and individual control types

Compatibility

The information on compatibility as described in the readme file also applies to SIMATIC CFC V8.0+SP2 incl. Update 1 (see attached file "Readme_CFC_V80_SP2_Upd1.zip").

Installation

The precondition for SIMATIC CFC V8.0+SP2 incl. Update 1 is that Update 1 or higher is installed for the Technological Hierarchy (TH) V8.0. Update 2 for the TH V8.0 is part of the download file of SIMATIC CFC V8.0+SP2 incl. Update 1 (see Download entry ID 62883989).

Important!
Before proceeding with the installation please read the Product Information in the readme file for SIMATIC CFC V8.0+SP2 incl. Update 1 and TH V8.0 Update 2 (see attached file "Readme_CFC_V80_SP2_Upd1.zip").

Readme_CFC_V80_SP2_Upd1.zip ( 77 KB )

Note: We also wish to bring to your attention that when you use "AS-OS Engineering" (WinCC compiler) the installed CFC software must always have the identical version.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.