×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 63481236, Entry date: 04/25/2017
(26)
Rate

Communication via OPC UA with SIMATIC HMI systems (Comfort Panels, Runtime Advanced, Runtime Professional)

  • Entry
  • Associated product(s)
OPC UA is a manufacturer-independent standard via which systems and devices of different manufactures can exchange their data with each other.

In the automation world, there are various, often vendor-dependent, communication interfaces. Nevertheless, systems and devices from different manufacturers have to exchange their data with each other. OPC UA is a cross-vendor standard that allows field devices to communicate with each other.

Solution
Many SIMATIC HMI systems support the communication via OPC UA. The application examples show various configurations for this purpose. An example project is available for each configuration.

The figure below shows a schematic illustration of the most important components for the
"02 - Panel Server and RT Advanced Client" configuration.
The Comfort Panel (server) provides the data. The PC station (client) accesses the data (tags) of the Comfort Panel.
The OPC UA communication interface supports data integrity through encryption and digital signature.


View configuration example 02

Documentation and example projects

  1. OPC UA Basics
    General information on the topic of OPC UA.
      Documentation (904,8 KB)

  2. Panel Server and RT Advanced Client
    communication between a panel that is configured as server and a Runtime Advanced that is configured as “client".
      Documentation (1,5 MB)
     Registrierung notwendig  Project (17,3 MB)

  3. S7-1500 Server and Panel Client
    communication between a SIMATIC S7-1500 controller that is configured as server and a panel that is configured as “client".
      Documentation (1,7 MB)
     Registrierung notwendig  Project (13,6 MB)

  4. Panel Server and OPC Scout Client
    communication between a panel that is configured as server and an OPC Scout that is configured as “client"
      Documentation (1,9 MB)
     Registrierung notwendig  Project (14,6 MB)

  5. RT Advanced Server and Panel Client
    communication between a Runtime Advanced that is configured as server and a panel that is configured as “client".
      Documentation (1,6 MB)
     Registrierung notwendig  Project (23,3 MB)

  6.  RT Professional Server and Panel Client
    communication between a Runtime Professional that is configured as server and a panel that is configured as “client".
      Documentation (1,6 MB)
     Registrierung notwendig  Project (37,5 MB)

Last Changes
complete revision


Additional Keywords
Data exchange, OPC-UA, operator panel, operating devices, OPC, connectivity, accessibility, access, interconnection
 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.