×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 637268, Entry date: 11/22/2000
(0)
Rate

Behavior of the S7-400 CPs when loading the HW Config

  • Entry
  • Associated product(s)


QUESTION:
Do all the S7-400 CPs behave in the same way when loading the HW Config?

ANSWER:
No. To a certain extent the S7-400 CPs behave differently when loading the HW Config if these CP modules are not networked. There are no differences if the modules are networked.

SIMATIC NET-CP

MLFB

Message when loading

CP status after loading

CP 443-5 Basic

6GK7 443-5FX00-0XE0

Message: Module is still not assigned to a network

STOP with error

6GK7 443-5FX01-0XE0

Message: Module is still not assigned to a network

Configuration data in the CPU

Configuration data in the CP

STOP with error

STOP with error

CP 443-5 Extended

6GK7 443-5DX00-0XE0

Message: Module is still not assigned to a network

RUN, after power OFF/ON STOP with error

6GK7 443-5DX01-0XE0

Message: Module is still not assigned to a network

RUN, after power OFF/ON STOP with error

6GK7 443-5DX02-0XE0

Message: Module is still not assigned to a network

STOP with error

CP 443-1 Basic

6GK7 443-1BX00-0XE0

Message: Module is still not assigned to a network

STOP with error

CP 443-1 TCP

6GK7 443-1EX00-0XE0

Message: Module is still not assigned to a network

STOP with error

CP 443-1 Basic/TCP

6GK7 443-1EX02-0XE0

Message: Module is still not assigned to a network

Configuration data in the CPU

Configuration data in the CP

STOP with error

STOP with error

6GK7 443-1EX10-0XE0

Message: Module is still not assigned to a network

Configuration data in the CPU

Configuration data in the CP

RUN, after power OFF/ON STOP with error

STOP with error

CP 443-1 IT

6GK7 443-1GX00-0XE0

Message: Module is still not assigned to a network

STOP with error

6GK7 443-1GX10-0XE0

Message: Module is still not assigned to a network

Configuration data in the CPU

Configuration data in the CP

RUN, after power OFF/ON STOP with error

STOP with error

Note:
Before loading the HW Config the CPU and CP are in RUN.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.