×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 63878336, Entry date: 09/18/2012
(0)
Rate

Update 3 for WinCC V7.0 SP3 and WinCC V7.0 SP3 ASIA also released for SIMATIC PCS 7 V8.0 + Update 1

  • Entry
  • Associated product(s)

Update 3 for WinCC V7.0 SP3 and WinCC V7.0 SP3 ASIA (see entry ID 63472422) is herewith also released for all ES/OS stations of the SIMATIC PCS 7 process control system with system software V8.0 + Update 1. For details on Update 3 for WinCC V7.0 SP3 and WinCC V7.0 SP3 ASIA please read the file "WinCC_V70_SP3_Update3_Readme.pdf" in entry ID 63472422.

Depending on the installed base, one of the following update versions must be used:

  • Update 3 for WinCC V7.0 SP3 with ES/OS software SIMATIC PCS 7 V8.0+Update 1
  • Update 3 for WinCC V7.0 SP3 ASIA with ES/OS software SIMATIC PCS 7 V8.0+Update 1 ASIA

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.