×
Siemens Industry Online Support
Siemens AG
Type de contribution : FAQ ID de la contribution : 64351747, Date de la contribution : 03/11/2015
(3)
Évaluer

What are the article numbers of the backup batteries for SIMATIC IPCs and SIMATIC Field PGs?

  • Contribution
  • Concerne le/les produits(s)
Backup batteries are used to maintain basic functions in the case of a power failure. We explain here how you can determine the article number of the backup battery of your SIMATIC IPC or SIMATIC Field PG.

Description
The backup battery of your SIMATIC IPC or SIMATIC Field PG is for maintaining basic function in the case of a power failure.

If the battery starts to run out, the diagnostics software SIMATIC IPCDiagMonitor or SIMATIC IPC DiagBase issues a diagnostics measure in good time before the battery runs out completely.

Remedy
In order to restore the function of the backup battery, you must replace the used battery with a new one.

When you disconnect the device from the power supply for replacing the backup battery, you must save the current BIOS settings in the BIOS Setup under "Save User Profile". After replacing the backup battery, you restore the settings you have just saved via "Load User Profile".

You can find the backup battery required for your SIMATIC IPC or SIMATIC Field PG under "Spares on Web" at the following link:

Spares on Web

There you enter the article number of your SIMATIC IPC or SIMATIC Field PG in the Article No.: input field and start the search for spare parts.

How to replace the backup battery, is described in the relevant device manual.

Additional Keywords
Order number, Mainboard, Motherboard, Battery, Lithium, CR2450N, CR1/2AA, Date, Lose, Forget

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport