×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 64351747, Entry date: 11/03/2015
(4)
Rate

What are the article numbers of the backup batteries for SIMATIC IPCs and SIMATIC Field PGs?

  • Entry
  • Associated product(s)
Backup batteries are used to maintain basic functions in the case of a power failure. We explain here how you can determine the article number of the backup battery of your SIMATIC IPC or SIMATIC Field PG.

Description
The backup battery of your SIMATIC IPC or SIMATIC Field PG is for maintaining basic function in the case of a power failure.

If the battery starts to run out, the diagnostics software SIMATIC IPCDiagMonitor or SIMATIC IPC DiagBase issues a diagnostics measure in good time before the battery runs out completely.

Remedy
In order to restore the function of the backup battery, you must replace the used battery with a new one.

When you disconnect the device from the power supply for replacing the backup battery, you must save the current BIOS settings in the BIOS Setup under "Save User Profile". After replacing the backup battery, you restore the settings you have just saved via "Load User Profile".

You can find the backup battery required for your SIMATIC IPC or SIMATIC Field PG under "Spares on Web" at the following link:

Spares on Web

There you enter the article number of your SIMATIC IPC or SIMATIC Field PG in the Article No.: input field and start the search for spare parts.

How to replace the backup battery, is described in the relevant device manual.

Additional Keywords
Order number, Mainboard, Motherboard, Battery, Lithium, CR2450N, CR1/2AA, Date, Lose, Forget

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.