×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 64847781, Entry date: 10/13/2021
(154)
Rate

Compatibility Tool for Automation and Drive Technology

  • Entry
  • Associated product(s)
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

Compatibility Tool
With this tool, you can easily get the compatibility statements for your automation and drive technology. The tool supports you in questions regarding the compatibility of various hardware and software products.

Needless to say, that you can download your compatibility lists for your individual product lines as an Excel file. 

Note: The database is constantly being revised and extended.

Brief instructions:

  1. First choose a "master component“ (WinCC, PCS 7, STEP 7, ...)
  2. Then add further components (e.g., operating systems, virus scanners, …)
  3. Now click on the "Show Compatibility" button
  4. The compatibility statement is displayed immediately

A detailed description of the tool is available in the Online help in the following table.


Contents
Link to the Compatibility Tool
German: http://www.siemens.de/kompatool
English: http://www.siemens.com/kompatool
Language-dependent link to the Compatibility Tool
https://support.industry.siemens.com/kompatool/index.html?lang=en
Documentation
Online Help.pdf (1.6 MB)

Table 1

Example Videos

  • Product families in the compatibility list



  • General operation

This video introduces you to the new functions in the Compatibility Tool.

  • Selection of an operating system as "Main Product"
  • Display of the latest release of the last two main versions
  • Automatic recognition and testing of the installed products



  • Manual compatibility check

This video shows you the ways of manually checking compatibility using an example.
In this example we use WinCC, STEP 7, an operating system and a virus scanner. You can extend the list to suit your requirements.

 

 


  • Download of compatibility lists and other useful applications

This video introduces you to the new functions in the Compatibility Tool.

 

 

Compatibility Tool revision history
The table below shows you the changes made in the past three months (data status and software functions).
  

StatusData Update
08/2021
New compatibility statements regarding software products:
  • PCS 7: V9.1, V9.0 SP3, V9.0 SP2, V9.0 SP1, V9.0, V8.2 SP1, V8.2
  • PCS neo: V3.1
  • PM-AGENT: V6.8
  • PM-CONTROL: V11.9
  • PM-LOGON: V1.8
  • PM-MAINT: V10.8
  • PM-OPEN EXPORT: V8.7
  • PM-OPEN IMPORT: V7.7
  • PM-QUALITY: V10.8
  • SIMATIC NET PC Software: V16.0 Upd4, V16.0 Upd3
  • SIMATIC Virtualization as a Service (SIVaaS): V3.6, V3.5 SP1
  • SIMIT: V10.3 Upd1, V10.3
  • SIMOCODE pro PCS 7 Library: V9.1
  • SIMOCODE pro PCS 7 Library Migration: V9.1
  • SINAUT ST7cc: V3.1 SP5
  • STEP 7 Basic (TIA Portal): V17.0, V16.0
  • STEP 7 Professional (TIA Portal): V17.0, V16.0
  • TeleControl Server Basic: V3.1 Upd3
  • WinCC: V7.5 SP2, V7.5 SP1, V7.5, V7.4 SP1, V7.4
  • WinCC Basic (TIA Portal): V17.0, V16.0
  • WinCC Comfort/Advanced (TIA Portal): V17.0, V16.0
  • WinCC RT Advanced (TIA Portal): V17.0, V15.1
  • WinCC Unified Engineering (TIA Portal): V17.0
07/2021
New compatibility statements regarding software products:
  • PCS 7: V9.1, V9.0 SP3, V9.0 SP2, V9.0 SP1, V9.0, V8.2 SP1, V8.2
  • STEP 7 Basic (TIA Portal)V17.0
  • WinCC Basic (TIA Portal): V17.0
  • WinCC Comfort/Advanced (TIA Portal): V17.0
  • WinCC Professional (TIA Portal): V17.0
  • WinCC RT Advanced (TIA Portal): V17.0
  • WinCC RT Professional (TIA Portal): V17.0
  • WinCC Unified  PC RT (TIA Portal): V17.0
  • WinCC Unified Engineering (TIA Portal): V17.0
06/2021
New compatibility statements regarding software products:
  • 3RW5 Soft Starter PCS 7 Library: V9.0 SP3
  • PCS 7: V9.1, V9.0 SP3
  • PM-CONTROL: V11.9
  • PM-LOGON: V1.8
  • PM-QUALITY: V10.8
  • SIMIT: V10.2 Upd2, V10.2 Upd1, V10.2
  • SIMOCODE pro PCS 7 Library Migration: V9.0 SP3
  • STEP 7 Basic (TIA Portal): V17.0, V16.0, V15.1, V15.0, V14.0 SP1
  • STEP 7 Professional (TIA Portal): V17.0, V16.0, V15.1, V15.0, V14.0 SP1
  • Teamcenter Gateway (TIA Portal): V17.0, V15.1 Upd6
  • WinCC: V7.5 SP2, V7.5 SP1, V7.5, V7.4 SP1, V7.4, V7.3 SE Upd1, V7.3, V7.2
  • WinCC Basic (TIA Portal): V17.0
  • WinCC Comfort/Advanced (TIA Portal): V17.0
  • WinCC Professional (TIA Portal): V17.0
  • WinCC RT Advanced (TIA Portal): V17.0
  • WinCC RT Professional (TIA Portal): V17.0
  • WinCC Unified  PC RT (TIA Portal): V17.0
  • WinCC Unified Engineering (TIA Portal): V17.0

New compatibility statements regarding hardware products:
  • Interface Modules: IM360 IM ZG, MIT K-BUS (6ES7360-3AA01-0AA0), IM361 IM EG, MIT K-BUS (6ES7361-3CA01-0AA0), IM365, OHNE K-BUS (6ES7365-0BA01-0AA0)
  • ET 200S: IM 151-1: IM 151-1 Basic (6ES7151-1CA00-0AB0), IM 151-1 Compact 16DI/16DO (6ES7151-1CA00-3BL0), IM 151-1 Compact 32DI (6ES7151-1CA00-1BL0), IM 151-1 FO (6ES7151-1AB02-0AB0), IM 151-1 FO Standard (6ES7151-1AB05-0AB0), IM 151-1 HF (6ES7151-1BA02-0AB0), IM 151-1 Standard (6ES7151-1AA04-0AB0), IM 151-1 Standard (6ES7151-1AA05-0AB0), IM151-1 STD, 12MBIT/S, SIMATIC DP (6ES7151-1AA06-0AB0)
  • ET 200S: IM 151-3 PN: IM 151-3  PN FO (6ES7151-3BB23-0AB0), IM 151-3  PN FO (6ES7151-3BB23-0AB0), IM 151-3  PN HF (6ES7151-3BA23-0AB0), IM 151-3  PN HF (6ES7151-3BA23-0AB0), IM 151-3  PN HF (6ES7151-3BA23-0AB0), IM 151-3  PN ST (6ES7151-3AA23-0AB0), IM 151-3  PN ST (6ES7151-3AA23-0AB0), IM 151-3  PN ST (6ES7151-3AA23-0AB0), IM 151-3 PN FO (6ES7151-3BB22-0AB0), IM 151-3 PN HF (6ES7151-3BA22-0AB0), IM 151-3 PN HS (6ES7151-3BA60-0AB0), IM 151-3 PN ST (6ES7151-3AA22-0AB0)
  • ET 200SP: Communication Modules: IO Link Master Module (6ES7137-6BD00-0BA0)
  • ET 200SP: IM155-6: IM 155-6 DP HF (6ES7155-6BU00-0CN0), IM 155-6 DP HF (6ES7155-6BU00-0CN0), IM 155-6 PB HF (6ES7155-6BU00-0CN0), IM 155-6 PN BA (6ES7 155-6AR00-0AN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN HF (6ES7155-6AU00-0CN0), IM 155-6 PN ST (6ES7155-6AU00-0BN0), IM 155-6 PN ST (6ES7155-6AU00-0BN0), IM 155-6 PN ST (6ES7155-6AU00-0BN0), IM 155-6 PN ST (6ES7155-6AU00-0BN0), IM 155-6 PN ST (6ES7155-6AU01-0BN0), IM 155-6 PN/2 HF (6ES7155-6AU01-0CN0), IM 155-6 PN/3 HF (6ES7155-6AU30-0CN0), IM155-6PN HS (6ES7155-6AU00-0DN0)
  • Fail-safe-CPUs (ET 200pro): IM 154-8F CPU (6ES7154-8FB01-0AB0), IM 154-8FX PN/DP CPU (6ES7154-8FX00-0AB0)
  • IM 151-7 CPU: IM 151-7 CPU FO, 48kB (6ES7151-7AB00-0AB0), IM 151-7 CPU, 96kB (6ES7151-7AA20-0AB0), IM 151-7 CPU, 128kB (6ES7151-7AA21-0AB0)
  • IM 151-7 F-CPU (ET 200S): IM 151-7 F-CPU (6ES7151-7FA20-0AB0), IM 151-7 F-CPU (6ES7151-7FA21-0AB0)
  • IM 151-8 F PN/DP CPU (ET 200S): IM 151-8F PN/DP CPU (6ES7151-8FB00-0AB0), IM 151-8F PN/DP CPU (6ES7151-8FB01-0AB0)
  • IM 151-8 PN/DP CPU: IM 151-8 PN/DP CPU, 128kB (6ES7151-8AB00-0AB0), IM 151-8 PN/DP CPU, 128kB (6ES7151-8AB01-0AB0)
  • IM 153-1 / IM 153-2: PROFIBUS-DP IM153-2 (6ES7153-2BA02-0XB0)
  • IM 153-4 PN IO: IM153-4 PN IO für 12 Module S7-300 (6ES7153-4AA01-0XB0), IM153-4 PN IO für 12 Module S7-300 (6ES7153-4AA01-0XB0), IM153-4 PN IO für 12 Module S7-300 (6ES7153-4AA01-0XB0), IM153-4 PN IO HF für 12 Module S7-300 (6ES7153-4BA00-0XB0), IM153-4 PN IO HF für 12 Module S7-300 (6ES7153-4BA00-0XB0)
  • IM 155-5 DP: IM 155-5 DP ST (6ES7155-5BA00-0AB0), IM 155-5 DP ST (6ES7155-5BA00-0AB0)
  • IM 155-5 PN: IM 155-5 PN BA (6ES7155-5AA00-0AA0), IM 155-5 PN BA (6ES7155-5AA00-0AA0), IM 155-5 PN HF (6ES7155-5AA00-0AC0), IM 155-5 PN HF (6ES7155-5AA00-0AC0), IM 155-5 PN HF (6ES7155-5AA00-0AC0), IM 155-5 PN HF (6ES7155-5AA00-0AC0), IM 155-5 PN ST (6ES7155-5AA00-0AB0), IM 155-5 PN ST (6ES7155-5AA00-0AB0), IM 155-5 PN ST (6ES7155-5AA00-0AB0), IM 155-5 PN ST (6ES7155-5AA01-0AB0)
  • Interface modules (ET 200AL): IM 157-1 DP (6ES7157-1AA00-0AB0), IM 157-1 PN (6ES7157-1AB00-0AB0)
  • Interface modules IM 154-1 DP und IM 154-2 DP: IM 154-1  DP (6ES7154-1AA01-0AB0), IM 154-1  DP (6ES7154-1AA01-0AB0), IM 154-1 DP (6ES7154-1AA00-0AB0), IM 154-2 DP  HF (6ES7154-2AA01-0AB0), IM 154-2 DP  HF (6ES7154-2AA01-0AB0), IM 154-2 DP HF (6ES7154-2AA00-0AB0)
  • Interface modules IM 154-3 PN und IM 154-4 PN: IM 154-3 PN HF Cu (6ES7154-3AB00-0AB0), IM 154-4 PN HF Cu (6ES7154-4AB10-0AB0), IM 154-4 PN HF Cu (6ES7154-4AB10-0AB0), IM 154-4 PN HF Cu (6ES7154-4AB10-0AB0), IM 154-4 PN HF Cu (6ES7154-4AB10-0AB0), IM 154-4 PN HF FO (6ES7154-4AB10-0AB0), IM 154-4 PN HF FO (6ES7154-4AB10-0AB0), IM 154-4 PN HF FO (6ES7154-4AB10-0AB0)
  • Interface modules IM 154-6 PN IWLAN: IM 154-6 PN HF  WLAN (6ES7154-6AB50-0AB0), IM 154-6 PN HF WLAN (6ES7154-6AB00-0AB0)
  • Standard-CPUs (ET 200pro): IM 154-8 PN/DP CPU 256kB (6ES7154-8AB01-0AB0)
Table 2

Additional Keywords
2334224, 6944907, 5895889, 6248329, 8250891, 8795716, 9061581, 9859007, 10154608, 11703924, 15082268, 15082926, 15093580, 15227707, 18734363, 19378505, 21169761, 21649775, 21852809, 21927667, 21927773, 21954341, 22055368, 22055716, 22056585, 24122009, 24254820, 25092587, 26998997, 31592453, 33912473, 37208360, 37571060, 40357341, 41306596, 49382005, 49382338, 49383047, 49385278, 49452605, 49453265, 49455057, 51120883, 51694087, 52255904, 67653438, .NET Framework, 05/2000+SP2, 07/2001, 11/2002, 11/2003+SP1, Operating systems, Compact Flash, DOT NET, DOTNET Framework, Drive ES, Edition 2005+HF1, Edition 2006, Edition 2007, Edition 2008, FDA 21 CFR Part 11, Remote diagnostics, Remote control, Remote servicing, Releases, Third-party software, GMP, Upgrade, IE, iMAP, Internet Explorer, Communication requirements, Comparison Tool, Compatible, Compatibility, Compatibility list, Compatibility matrix, Compatibility tool, CompaTool, Life Science, McAfee VirusScan, Migration, MS .NET, PCS 7 Migration OS Options, Pharma, ProTool, RAID System, S7, SIMATIC PC BIOS Manager, SIMATIC PC DiagMonitor, SIMATIC PC Image & Partition Creator, SIMOTION Scout, SmartTools, SSD, PCS7, STEP7, Symantec AntiVirus, SIMATIC NET, System requirements, TIA Portal, Trend Micro Office Scan, Overview, V12, V8.0, V8.1, V8.2, Validation, Version, Virus scanner, Vista, WebNavigator, Win7, Win8, WinAC RTX, Windows 2000 Professional, Windows 2003 Server, Windows 2008 Server, Windows 7, Windows 8, Windows 98, Windows operating system, Windows ME, Windows NT, Windows Seven, Windows Vista, Windows XP, Windows 10, Feature Update, Funktions Update, LTSB, Long Time Service Brach,LTSC, Long Time Service Channel, Windows version, XP, Additional software

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.